Importing EdDSA (ED25519) public key into S32K3 HSE for verification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Importing EdDSA (ED25519) public key into S32K3 HSE for verification

331 Views
elbartospringfield
Contributor I

Hi NXP Community,

Use case:

Use private key on PC side to sign some data, use public key on S32K3 side to verify data.

Key pair generation done with OpenSSL:

 

 

openssl genpkey -algorithm Ed25519 -outform PEM -out private_key.pem
openssl pkey -in private_key.pem -pubout -outform PEM -out public_key.pem

 

 

Listing the key contents with OpenSSL produces the following output (these keys are valid of course, but considered dummy for demo purposes only):

 

 

openssl pkey -inform pem -in private_key.pem -text

-----BEGIN PRIVATE KEY-----
MC4CAQAwBQYDK2VwBCIEINpkm+ArI/HFbCgWttsHNHS0jW1fwI5GhnIxAoXG4S0i
-----END PRIVATE KEY-----
ED25519 Private-Key:
priv:
    da:64:9b:e0:2b:23:f1:c5:6c:28:16:b6:db:07:34:
    74:b4:8d:6d:5f:c0:8e:46:86:72:31:02:85:c6:e1:
    2d:22
pub:
    65:9c:25:9c:4b:e0:5f:46:5c:b7:12:52:91:86:7c:
    d8:dc:96:d5:11:90:8c:65:8d:b2:f3:c7:2f:66:2e:
    6e:6b

 

 

Public key is transformed into an array as follows:

 

 

unsigned char eddsa_public_key[] = {
        0x6B, 0x6E, 0x2E, 0x66, 0x2F, 0xC7, 0xF3, 0xB2, 
        0x8D, 0x65, 0x8C, 0x90, 0x11, 0xD5, 0x96, 0xDC, 
        0xD8, 0x7C, 0x86, 0x91, 0x52, 0x12, 0xB7, 0x5C,
        0x46, 0x5F, 0xE0, 0x4B, 0x9C, 0x25, 0x9C, 0x65 };

 

 

The key catalog is then formatted according to the following scheme:

 

 

/** @brief  HSE NVM key catalog configuration */
#define  HSE_NVM_KEY_CATALOG_CFG  \
        /* Group MU Mask   Group Owner          Group Key Type              Number of Slots     Maximum slot size (in bits)  */ \
        /* CUST keys */                                                                                                         \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES,            3U,                 HSE_KEY256_BITS,    {0U} },    \
        /* HMAC key */                                                                                                          \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_HMAC,           1U,                 HSE_KEY512_BITS,    {0U} },    \
        /* ECC keys */                                                                                                          \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR,       2U,                 HSE_KEY256_BITS,    {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PUB,        1U,                 HSE_KEY256_BITS,    {0U} },    \
        /* RSA keys */                                                                                                          \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PAIR,       3U,                 HSE_KEY4096_BITS,   {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PUB,        4U,                 HSE_KEY4096_BITS,   {0U} },    \
        { 0U,               0U,                 0U,                          0U,                 0U,                 {0U} }

/** @brief  HSE RAM key catalog configuration */
#define  HSE_RAM_KEY_CATALOG_CFG                                                                                                \
        /* Group MU Mask   Group Owner          Group Key Type              Number of Slots     Maximum slot size (in bits)  */ \
        /* Symmetric key */                                                                                                     \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_AES,           6U,                 HSE_KEY128_BITS,    {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_AES,           3U,                 HSE_KEY192_BITS,    {0U} },    \
        /* Usable only on MU1 */                                                                                                \
        { GRANT_COD_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_AES,           3U,                 HSE_KEY256_BITS,    {0U} },    \
        /* HMAC key */                                                                                                          \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_HMAC,          6U,                 HSE_KEY1024_BITS,   {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_HMAC,          2U,                 HSE_KEY256_BITS,    {0U} },    \
        /* ECC keys*/                                                                                                           \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_ECC_PAIR,      2U,                 HSE_KEY521_BITS,    {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_ECC_PUB,       6U,                 HSE_KEY521_BITS,    {0U} },    \
        /* Temporary secrets */                                                                                                 \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_SHARED_SECRET, 1U,                 HSE_KEY638_BITS,    {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_SHARED_SECRET, 2U,                 HSE_KEY2048_BITS,   {0U} },    \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_SHARED_SECRET, 2U,                 HSE_KEY4096_BITS,   {0U} },    \
        /* RSA keys */                                                                                                          \
        { GRANT_ALL_ACCESS, HSE_KEY_OWNER_ANY,   HSE_KEY_TYPE_RSA_PUB,       3U,                 HSE_KEY4096_BITS,   {0U} },    \
        { 0U,               0U,                  0U,                         0U,                 0U,                 {0U} }

 

 

A pair of ECC (EdDSA) keys are generated and accommodated in HSE_NVM_KEY_CATALOG_CFG (2, 0).

The public key shown above is imported successfully in HSE_NVM_KEY_CATALOG_CFG (3, 0).

To test the generated key-pair, a signature is verified over the following trivial array:

 

 

const char helloTest[5] = {'h','e','l','l','o'};

 

 

The array is signed with the private key from HSE_NVM_KEY_CATALOG_CFG (2,0) and then it is verified with the public key from the same slot. This works fine.

Now the problem start.

To test the key-pair generated with OpenSSL (shown above), the following steps are taken:

 

printf "%s" "hello" > hello.bin

openssl pkeyutl -sign -inkey private_key.pem -rawin -in hello.bin -out hello.bin.sig

openssl pkeyutl -verify -pubin -inkey public_key.pem -rawin -in hello.bin -sigfile hello.bin.sig
Signature Verified Successfully

 

The signature produced is:

 

xxd -i hello.bin.sig
unsigned char hello_bin_sig[] = {
  0x57, 0x24, 0xbf, 0xf8, 0x28, 0xa6, 0x54, 0xf3, 0x52, 0x4e, 0xf7, 0x0e,
  0xc2, 0xd7, 0x0b, 0xf9, 0x06, 0x3f, 0xe7, 0x17, 0xe0, 0x48, 0x6f, 0xe4,
  0xa0, 0xa7, 0xaa, 0x7e, 0x15, 0x26, 0x26, 0xa6, 0x47, 0xb7, 0xb8, 0x1a,
  0x2f, 0x60, 0x3d, 0x4e, 0x00, 0xb7, 0x42, 0x1a, 0x69, 0xa8, 0x17, 0x03,
  0x35, 0xd2, 0xa2, 0x9f, 0xe1, 0x60, 0x8e, 0x8a, 0x41, 0x47, 0x5d, 0x8d,
  0xbc, 0x81, 0x51, 0x05
};
unsigned int hello_bin_sig_len = 64;

 

 

The hello_bin_sig array is now split up into the r and s parts (32 byte each) and fed into the same Verify-function used previously (when I was testing the generated key pair), only this time using the public key that was installed in HSE_NVM_KEY_CATALOG_CFG (3, 0). The verification fails, returning HSE_SRV_RSP_VERIFY_FAILED ((hseSrvResponse_t)0x55A5A164UL).

Any ideas on what I might be doing wrong here?

BR

Tags (2)
0 Kudos
Reply
2 Replies

278 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @elbartospringfield 

See please attached document. It thoroughly explains how to generate ECC key pair in openssl and how to use it in HSE.

Regards,

Lukas

272 Views
elbartospringfield
Contributor I
Thanks @lukaszadrapa, I did find this example posted in a another thread and I can get this example to work with keys I've generated myself using openssl. I still can not get EdDSA to work. I would really appreciate if the example you provided could be re-worked to use EdDSA (HSE_EC_25519_ED25519).
0 Kudos
Reply