IVT with HSE FW on S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IVT with HSE FW on S32K344

ソリューションへジャンプ
1,215件の閲覧回数
IAussman
Contributor III

Dear NXP community,

I would like to know if IVT is mandatory for making use of HSE FW.

From my understanding, the main purpose of IVT is to specify the base address of HSE FW pink when flashing it.

NXP provides only the IVT that is demo-application specific so we cannot use it in another application.

If the IVT is mandatory, how can we generate another one for our application ?

My second question is, if I flash the NXP demo-application with IVT, can I erase it with my own application  later ?

Thank you in advance for your support.

Aussman

 

0 件の賞賛
返信
1 解決策
1,200件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @IAussman 

HSE FW can be installed either using IVT or without IVT.

We provide document AN744810 “HSE FW install for S32K3xx” which describes how to install the firmware. It can be found in Documentation in Secure Files section:

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

 

lukaszadrapa_0-1682089520670.png

 

 This corresponds to description from Readme file from HSE DEMOAPP package:

lukaszadrapa_1-1682089575559.png

Even if you use IVT method, you can erase it after installation / replace it with own application with own IVT.

Regards,

Lukas

元の投稿で解決策を見る

2 返答(返信)
1,201件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @IAussman 

HSE FW can be installed either using IVT or without IVT.

We provide document AN744810 “HSE FW install for S32K3xx” which describes how to install the firmware. It can be found in Documentation in Secure Files section:

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

 

lukaszadrapa_0-1682089520670.png

 

 This corresponds to description from Readme file from HSE DEMOAPP package:

lukaszadrapa_1-1682089575559.png

Even if you use IVT method, you can erase it after installation / replace it with own application with own IVT.

Regards,

Lukas

1,196件の閲覧回数
IAussman
Contributor III
Hi Lukas,
Thanks for your response.
Best regards,
Aussman
0 件の賞賛
返信