I2C Bit Bang example with S32K1xx series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Bit Bang example with S32K1xx series

Jump to solution
2,002 Views
Learner
Contributor III

Hi 

As per my project needs, i need to have I2C bit banging. Is there any reference I2C bit banging example code available for S32K1xx series of microcontroller?

Tags (1)
0 Kudos
Reply
1 Solution
1,951 Views
Learner
Contributor III
0 Kudos
Reply
4 Replies
1,998 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

as far as I know it is not available.  But you can refer to https://community.nxp.com/t5/S32K/S32K116-GPIO-emulate-I2C/m-p/1079549.

 

BR, Petr

0 Kudos
Reply
1,981 Views
Learner
Contributor III

Hi @PetrS 

Thanks for your reply.

Shared community link is referencing an application note i.e. AN5264.

And AN5264 is referring files attachments but there is no file attached with application note.

please help me to get the attachment of Application Note AN5264 

0 Kudos
Reply
1,969 Views
PetrS
NXP TechSupport
NXP TechSupport
1,952 Views
Learner
Contributor III

 @PetrS  Thanks 

0 Kudos
Reply