Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

720件の閲覧回数
mahdikazemi12
Contributor I

Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

1 返信

656件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if we are talking about these development kits:

S32K144 3-phase PMSM Development Kit|NXP 

S32K144 3-phase BLDC Development Kit|NXP 

... then power supply is included in the package and the parameters are 12V and 5A.

Regards,

Lukas