Failed to load falsh loader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to load falsh loader

411件の閲覧回数
shivakrishna
Contributor I

I am having an issue with the flash the software.

I get an error when trying to download using I-Jet.

i am using S32K312 controller.

The error message is:

Failed to load flash loader:C:\Program files(x86)\IAR Systems\Embedded Workbench 8.4 EWARM FS 8.50.10\arm\config\flashloader\NXP\FalshS32K3x2.flash

shivakrishna_0-1712047671010.png

shivakrishna_1-1712047684801.png

please help me to resolve this issue.

 

 

0 件の賞賛
返信
3 返答(返信)

373件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @shivakrishna 

what kind of board do you have? Is that our EVB or do you have your own design? Was it working in the past? If it is related to I-Jet configuration, please discuss this directly with IAR.

Regards,

Lukas

0 件の賞賛
返信

366件の閲覧回数
shivakrishna
Contributor I

hi NXP team,

Its our own design, and it was working properly in the past, 

and its not issue with I-jet, with same I-jet i flashed in other boards its flashing properly, 

can you please guide me how to resolve this issue.

0 件の賞賛
返信

355件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Did you try to measure all supply voltages? Is the reset deasserted after power on? Did you try to measure current consumption of good board and bad board to see if there's some significant difference (i.e. possible shortcut or something like that)?

What was the last operation / change in your software when it stopped working?

Regards,

Lukas

0 件の賞賛
返信