Clock config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock config

2,822 Views
rajesh057
Contributor III

Hi ,

I am trying to config clock 80 Mhz ,my external clock 16 Mhz ,I have configured like below pic ...getting TIME_OUT FROM return status from

CLOCK_SYS_SetConfiguration() function .

Thanks

Rajesh K

5 Replies

2,608 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Rajesh,

The warning informs you that the SPLL_CLK frequency must be between 90 MHz and 160 MHz.

So, I recommend you to set the SPLL_CLK = 160 MHz and for SYS_CLK set SPLL_CLK/2. After that, you reach SYS_CLK = 80 MHz without warnings.

pastedImage_1.png

I hope it helps you.

If you have any questions, let me know.

Best Regards,

Diana

2,608 Views
rajesh057
Contributor III

hi Diana ,

Thanks for answer .

its is not related to the software issue its hardware problem .

on more problem I am facing with Latest SDK os millisecond function not working .interrupt not triggering.

Thanks

Rajesh Kota. 

0 Kudos
Reply

2,608 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Rajesh,

However, I have seen in your attachment a warning below because the PLL frequency is not within the range. 

pastedImage_1.png

Regarding your second question, could you please provide more information such as a piece of your code settings?

Thank you.

Best Regards,

Diana

0 Kudos
Reply

2,608 Views
rajesh057
Contributor III

Hi Razvan-nicolae Tilimpea

Thanks

Please find the following attachment.

SDK_Version.GIF

0 Kudos
Reply

2,608 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Can can you mention what is the SDK version used in your project?

Best regards,

Razvan

0 Kudos
Reply