Adc_example_S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adc_example_S32K344

500 Views
GaryZhang1
Contributor III

Which package I should install to have Adc_example_S32K344 available.

I have S32K3X4EVB-Q172 board and have installed: 

SW32K3xx.S32DS_3.5.0_D2303.zip,

SW32K3_RTD_4.4_R21-11_3.0.0_CD04_D2212_updatesite.zip, and 

SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip, 

I only see Adc_example_S32K311 available.

Thanks

Gary

I am able to get Adc_example_S32K344 now after install "SW32K3_RTD4.4_R21-11_3.0.0_D2303",

 

Issue:

When I build: "Adc_example_S32K344" or "Clock_Lp_Example_S32K344"

I have the same Error of "Pins initialization requires the PINS Driver in the project" after I enable the Pins configuration,

But I can build "Port_Example_S32K344" without error. 

Any advice?

Thanks

Gary

0 Kudos
Reply
3 Replies

427 Views
GaryZhang1
Contributor III

This is no longer an issue after updated the main.c code., thanks -- Gary

0 Kudos
Reply

493 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@GaryZhang1

from my side,

Senlent_0-1690983120246.png

 

0 Kudos
Reply

472 Views
GaryZhang1
Contributor III
Thanks for the reply.
0 Kudos
Reply