请问S32K14 系列的SPI最大波特率是多少

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

请问S32K14 系列的SPI最大波特率是多少

713 Views
xinyuan2023
Contributor I

请问S32K14 系列的SPI最大波特率是多少

0 Kudos
5 Replies

700 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos

691 Views
xinyuan2023
Contributor I
谢谢Senlent,想再和您确认一下:
(1)表格里的Peripheral Frequency是指SPLLDIV2_CLK这个时钟吗

(2)也就是说:在高速模式下 HSRUN Mode 使用3.3V供电
使用SPI的最大工作波特率是14MHZ(限LPSPI0),LPSPI1和LPSPI2是12MHZ。

谢谢!
0 Kudos

683 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@xinyuan2023

1.这个指的是外设时钟,外设时钟最高只能是由SPLLDIV2_CLK提供,所以你这么理解也可以

2.你可以看数据手册,应该是的

This is the maximum operating frequency (fop) for LPSPI0 with GPIO-HD PAD type only. Otherwise, the maximum operating frequency (fop) is 12 Mhz.

0 Kudos

672 Views
xinyuan2023
Contributor I
HI Senlent:
使用S32DS看SPI设置波特率的例程,一头雾水,SPLLDIV2_CLK之后应该是经过PRESCALE分频,之后通过CCR寄存器怎么得到的波特率就看不懂了,还请赐教,谢谢。
0 Kudos

680 Views
xinyuan2023
Contributor I
Senlent 再次感谢!
0 Kudos