processor are not defined for the project in s32ds on windows 11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

processor are not defined for the project in s32ds on windows 11

866 Views
adityakumar
Contributor I

I'm facing  problems in creating a new project in S32DS . I've downloaded external package and internally after installing and updating packages , I'm facing a problem related to "processor are not defined for the project" in s32ds on windows 11. Can anyone help me out ??

0 Kudos
Reply
1 Reply

856 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello adityakumar,

It means that the project that you download is not for S32DS, btw Windows 11 still under investigation since there are some issue, this can be one of them.My suggestion install it on Windows 10.

 

Regards

 

 

 

0 Kudos
Reply