Hi,All
I want to add some code to test leds , so I want to change s32gxxxa-rdb.dtsi.
Then I follows the steps:
delete directory :build_s32g274ardb2
cd fsl-auto-yocto-bsp
./sources/meta-alb/scripts/host-prepare.sh
. nxp-setup-alb.sh -m s32g274ardb2
bitbake fsl-image-auto
then I want to change dtsi, so I set the command:
devtool devtool modify linux-s32
in build_s32g274ardb2/workplace/sources/linux-s32/arch/arm64/boot/dts/freescale, I change dtsi.
Then I run the command:
devtool build linux-s32
it reports errors:
Then I want to fix it , I run the command:
bitbake -c cleansstate linux-s32
and I run:devtool build linux-s32, it still repots the same errors.
I want to custom the devicetree and build it to writing it to SD card.
What should I do to make it work or can anyone tell me the right steps?
Solved! Go to Solution.
Hi @Ada_Lovelace,
Please share the error log file here as can't understand the cause of error from the screenshot which you have attached.
Thanks,
Mayank s Patel
Hi @Ada_Lovelace,
Please share the error log file here as can't understand the cause of error from the screenshot which you have attached.
Thanks,
Mayank s Patel
HI,
I solved the problem, I use the wrong grammar about customing the devicetree, now I have corrected it.