Tresos Studio 27.1 can not open Bootloader_S32G2XX_ASR_4.4_M7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tresos Studio 27.1 can not open Bootloader_S32G2XX_ASR_4.4_M7

1,245 Views
junjie_wu_enjoymove
Contributor I

Hello Team,

We want to design M7 bootloader that should load M7_0 app and A53_0 U-boot. We are using Platform Software integration 21.04 and Tresos 27.1. We have followed the Bootloader manual installed relevant tools and software package(S32XX 4.4 1.0.0 HF1),But we can't use Tresos Studio 27.1 to open Bootloader_S32G2XX_ASR_4.4_M7,What steps did we do wrong? Can you help us?

0 Kudos
2 Replies

929 Views
asap
NXP Employee
NXP Employee

junjie_wu_enjoymove, bruce-lip,

To install the RTD (MCAL) module support in EB tool, you might refer to GoldVIP UM10.4 (step.3), here is a community post for more detail.

Albert
0 Kudos

992 Views
bruce-lip
Contributor I

I have the same problem. Is there any update ?

erro log

Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "MemDal_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"
Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "CryptoDal_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"
Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "SysDal_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"
Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "Bootloader_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"
Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "ComDal_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"
Project: Bootloader_S32G2XX_ASR_4.4_M7<br>Plug-in with a module "ComManager_TS_T40D11M217I0R0" is not installed - cannot create module configurations for project "Bootloader_S32G2XX_ASR_4.4_M7"

0 Kudos