Dear NXP expert,
I have tested the demo of '13.9 Ethernet bridge between M7 and A53' in 'GoldVIP-S32G3-1.11.0-User-Manual.pdf', however it does't work, the whole operation process attached. Could you please give me some suggestions to fix the problem? Some other information: M7 is able to receive the ARP packets from A53 and send the response.
解決済! 解決策の投稿を見る。
Hi,
We have received the following comments on regards of this situation:
"
Try to append the following command to boot.source and regenerate the boot.scr in /boot.
fdt rm /soc/pfe_slave@46000000/ethernet@104
Or modify the bootcmd environment variable of u-boot as the follows:
setenv bootcmd 'ext4load mmc ${mmcdev}:${mmcpart_ext} ${script_addr} boot/${script}; source ${script_addr}; fdt rm /soc/pfe_slave@46000000/ethernet@104; booti ${xen_addr} - ${fdt_addr};'
"
Please, let us know.
Hi,
Let us verify the information you have provided. Once we have an update, we will let you know.
We do apologize for the delay.
Please, let us know.
Hi Daniel,
Thanks for your reply. In the last days, I have also tested the GoldVIP images on S32G274ardb2 by contrast. The 'Ethernet bridge between M7 and A53' demo only works on the version of GoldVIP 1.8.0(pfe version 1.2.0 rc2, the normal dmesg attached below) in S32G2 platform, and all other versions failed including the newest 1.11.0. Unfortunately, I didn't find a GoldVIP version that works well on S32G399ardb3 until now. Please let me know if you find the root cause, thanks!
Hi,
Thanks for your feedback. We might be misunderstanding the request with this last comment.
When you implemented GoldVIP 1.11.0, which PFE version did you use? v1.2.0 rc2 or v1.3.0?
Can you help us understand which package versions are you using for GoldVIP 1.11.0?
Please, let us know.
Hi,
Thanks for your feedback. Seems odd that you are seeing that the GoldVIP v1.11.0 PFE-FW version is v1.6.0, since the following is shown under the GoldVIP User Manual:
In which PFE-FW is v1.8.0 and PFE driver is v1.3.0. If you are seeing that the PFE versions are not the same as the ones shown under the GoldVIP UM, there seems to be a problem with the images. We understand that they were built manually, is this correct?
Please, let us know.
Hi Daniel,
Thanks for your reply and I'm sorry for causing some misunderstandings between us. The PFE version I noted before is reading from the dmesgs of GoldVIP 1.11.0, in which the whole message is ‘pfeng-slave 46000000.pfe_slave: Version: 1.6.0’, you can see more in the attachment. And the image of GoldVIP 1.11.0 was just download from NXP's 'Automotive Software Package Manager', I didn't rebuild it at all. I couldn't figure whether the version of PFE firmware and the PFE driver is correct or not. Could you please just test the GoldVIP 1.11.0 on S32G3ardb3 with the images that NXP's official website released? I’m looking forward to your test results. If more information needed, please let me know.
Hi,
Thanks for your feedback. We will then verify the functionality for GoldVIP 1.11.0. Once we have any update we will let you know.
We apologize for any delay from our side.
Please, let us know.
Hi,
We have received the following comments on regards of this situation:
"
Try to append the following command to boot.source and regenerate the boot.scr in /boot.
fdt rm /soc/pfe_slave@46000000/ethernet@104
Or modify the bootcmd environment variable of u-boot as the follows:
setenv bootcmd 'ext4load mmc ${mmcdev}:${mmcpart_ext} ${script_addr} boot/${script}; source ${script_addr}; fdt rm /soc/pfe_slave@46000000/ethernet@104; booti ${xen_addr} - ${fdt_addr};'
"
Please, let us know.
Hi Daniel,
Thank you so much for the reply, the above solution did work by modifiing the bootcmd env. However, I'd like to try the first method to change the boot.soure as a permanent method, could you please give me some advice on how to generate the boot.source and boot.src from u-boot source code ? And another questions are why the '/soc/pfe_slave@46000000/ethernet@104' should be removed from the fdt and what does the 'ethernet@104' mean in pfe_slave?
Hi,
Thanks for your feedback. With this, we understand that everything is working now, is this correct?
As for your questions, we will confirm with the related team.
Please, let us know.
Hi,
We have received the following update:
"
U-boot.source is genereated by the patch file "sources/meta-alb/recipes-extended/imagebuilder/imagebuilder/0001-uboot-script-gen-Dynamically-compute-addr-and-size-w.patch".
I recommend modifying the kernel dts file for removing the ethernet@104:
removing the following section in file:
&pfesl_hif0 { status = "okay"; }; |
arch/arm64/boot/dts/freescale/s32g399a-rdb3-pfems.dts for s32g399ardb3, and
arch/arm64/boot/dts/freescale/s32g274a-rdb2-pfems.dts for s32g274ardb2.
There are 5 ethernet interfaces based on PFE: pfe0sl, pfe1sl, pfe2sl, hif0sl and aux0sl. They represent different packet links respectively, a PFE flexibility features. pfe0sl, pfe1sl and pfe2sl send and receive packets from MAC0, MAC1 and MAC2 of PFE respectively, hif0sl sends and receive packet from HIF0 of PFE, aux0sl receives all remain packets. So if hif0sl exists, packets from HIF0 (The M7 host core sends these packets in GoldVIP) will be received by hif0sl; if hif0sl dosen't exist, those packets will be received by aux0sl. Another way to avoid hif0sl receiving packets is adding "nxp,pfeng-netif-mode-mgmt-only" property to dts node relating to hif0sl. In this way , hif0sl only receives management packets , currently the management packets only contain PTP message packets, other packets will be received by aux0sl.
"
Please, let us know.
root@s32g399ardb3:~# dmesg | grep pfeng
[ 2.820608] pfeng_slave: loading out-of-tree module taints kernel.
[ 2.832437] pfeng-slave 46000000.pfe_slave: PFEng ethernet driver loading ...
[ 2.832453] pfeng-slave 46000000.pfe_slave: Version: 1.6.0
[ 2.832457] pfeng-slave 46000000.pfe_slave: Driver commit hash: M4_DRIVER_COMMIT_HASH
[ 2.832461] pfeng-slave 46000000.pfe_slave: Multi instance support: SLAVE/mdetect=on
[ 2.832466] pfeng-slave 46000000.pfe_slave: Compiled by: 11.4.0
[ 2.832869] pfeng-slave 46000000.pfe_slave: Wait for PFE controller UP ...
[ 2.832897] pfeng-slave 46000000.pfe_slave: PFE controller UP detected
[ 2.832904] pfeng-slave 46000000.pfe_slave: Cbus addr 0x46000000 size 0x1000000
[ 2.832914] pfeng-slave 46000000.pfe_slave: IHC channel: 3
[ 2.832920] pfeng-slave 46000000.pfe_slave: MASTER IHC channel: 0
[ 2.832930] pfeng-slave 46000000.pfe_slave: netif name: pfe0sl
[ 2.832937] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:00
[ 2.832947] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) linked phyif: 0
[ 2.832953] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) mode: std
[ 2.832988] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) HIFs: count 1 map 08
[ 2.832997] pfeng-slave 46000000.pfe_slave: netif name: pfe1sl
[ 2.833002] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:01
[ 2.833010] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) linked phyif: 1
[ 2.833014] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) mode: std
[ 2.833019] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) HIFs: count 1 map 08
[ 2.833028] pfeng-slave 46000000.pfe_slave: netif name: pfe2sl
[ 2.833033] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:02
[ 2.833040] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) linked phyif: 2
[ 2.833045] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) mode: std
[ 2.833050] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) HIFs: count 1 map 08
[ 2.833059] pfeng-slave 46000000.pfe_slave: netif name: aux0sl
[ 2.833064] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:80
[ 2.833070] pfeng-slave 46000000.pfe_slave: netif(aux0sl) no linked phyif in AUX mode
[ 2.833074] pfeng-slave 46000000.pfe_slave: netif(aux0sl) mode: aux
[ 2.833079] pfeng-slave 46000000.pfe_slave: netif(aux0sl) HIFs: count 1 map 08
[ 2.833088] pfeng-slave 46000000.pfe_slave: netif name: hif0sl
[ 2.833092] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:f0
[ 2.833099] pfeng-slave 46000000.pfe_slave: netif(hif0sl) linked phyif: 6
[ 2.833104] pfeng-slave 46000000.pfe_slave: netif(hif0sl) mode: std
[ 2.833109] pfeng-slave 46000000.pfe_slave: netif(hif0sl) HIFs: count 1 map 08
[ 2.833114] pfeng-slave 46000000.pfe_slave: HIF channels mask: 0x0008
[ 2.833152] pfeng-slave 46000000.pfe_slave: PFE port coherency enabled, mask 0x1e
[ 2.833210] pfeng-slave 46000000.pfe_slave: assigned reserved memory node pfebufs@83600000
[ 2.833225] pfeng-slave 46000000.pfe_slave: PFE CBUS p0x(____ptrval____) mapped @ v0xffffffc012000000
[ 2.833233] pfeng-slave 46000000.pfe_slave: Wait for Master UP ...
[ 2.833251] pfeng-slave 46000000.pfe_slave: Detected Master UP
[ 2.833273] pfeng-slave 46000000.pfe_slave: HIF3 is in clean state
[ 2.833474] pfeng-slave 46000000.pfe_slave: HIF0 not configured, skipped
[ 2.833480] pfeng-slave 46000000.pfe_slave: HIF1 not configured, skipped
[ 2.833484] pfeng-slave 46000000.pfe_slave: HIF2 not configured, skipped
[ 2.833832] pfeng-slave 46000000.pfe_slave: HIF3 enabled
[ 2.833842] pfeng-slave 46000000.pfe_slave: HIF3 started
[ 2.833847] pfeng-slave 46000000.pfe_slave: IDEX-slave @ master-interface 6
[ 2.833856] pfeng-slave 46000000.pfe_slave: IHC client registered
[ 2.837920] pfeng-slave 46000000.pfe_slave: IDEX: v2 protocol used, Resend:count=10,delay=100ms
[ 2.837929] pfeng-slave 46000000.pfe_slave: IDEX RPC installed on HIF3
[ 2.837973] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Subscribe to HIF3
[ 2.837999] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Subscribe to HIF3
[ 2.838004] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Host LLTX disabled
[ 2.838028] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Subscribe to HIF3
[ 2.838061] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Subscribe to HIF3
[ 2.838080] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Subscribe to HIF3
[ 2.838087] pfeng-slave 46000000.pfe_slave: MDIO bus 0 disabled: Not found in DT
[ 2.838092] pfeng-slave 46000000.pfe_slave: MDIO bus 1 disabled: Not found in DT
[ 2.838096] pfeng-slave 46000000.pfe_slave: MDIO bus 2 disabled: Not found in DT
[ 2.872316] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 5!=6. Skipped
[ 2.877438] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 6!=7. Skipped
[ 2.882569] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 7!=8. Skipped
[ 2.887678] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 8!=9. Skipped
[ 2.892798] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 9!=10. Skipped
[ 2.897664] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 10!=11. Skipped
[ 2.903142] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 11!=12. Skipped
[ 2.937775] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Enable HIF3
[ 2.975547] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 21!=22. Skipped
[ 2.976123] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): receive traffic matching its MAC address
[ 2.976135] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:00
[ 3.021135] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 28!=29. Skipped
[ 3.035298] pfeng-slave 46000000.pfe_slave pfe0sl: registered
[ 3.035344] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Host LLTX disabled
[ 3.094704] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Enable HIF3
[ 3.114884] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): receive traffic matching its MAC address
[ 3.114899] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:01
[ 3.178561] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 51!=52. Skipped
[ 3.180092] pfeng-slave 46000000.pfe_slave pfe1sl: registered
[ 3.180108] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Host LLTX disabled
[ 3.190533] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 53!=54. Skipped
[ 3.221343] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 58!=59. Skipped
[ 3.228370] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 59!=60. Skipped
[ 3.235507] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Enable HIF3
[ 3.258665] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): receive traffic matching its MAC address
[ 3.258683] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:02
[ 3.329888] pfeng-slave 46000000.pfe_slave pfe2sl: registered
[ 3.329909] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Host LLTX disabled
[ 3.357111] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Enable HIF3
[ 3.357596] pfeng-slave 46000000.pfe_slave aux0sl: checksum offload not possible for AUX interface
[ 3.357870] pfeng-slave 46000000.pfe_slave aux0sl: registered
[ 3.357882] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Host LLTX disabled
[ 3.385673] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 78!=79. Skipped
[ 3.386086] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Enable HIF3
[ 3.386827] pfeng-slave 46000000.pfe_slave hif0sl: registered
[ 11.720180] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 126!=127. Skipped
[ 11.727756] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 127!=128. Skipped
[ 11.740535] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 129!=130. Skipped
[ 11.744048] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 130!=131. Skipped
[ 12.001540] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 317!=318. Skipped
[ 12.009564] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 318!=319. Skipped
[ 12.012704] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 319!=320. Skipped
[ 12.033602] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 324!=325. Skipped
[ 12.036952] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 325!=326. Skipped
[ 12.058010] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 332!=333. Skipped
[ 12.105951] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 338!=339. Skipped
[ 12.125580] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 339!=340. Skipped
[ 12.125604] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 339!=340. Skipped
[ 12.136532] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 340!=341. Skipped
[ 12.146816] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 341!=342. Skipped
[ 12.157094] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 342!=343. Skipped
[ 12.185535] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 347!=348. Skipped
[ 12.185559] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 347!=348. Skipped
[ 12.205535] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 348!=349. Skipped
[ 12.209378] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 349!=350. Skipped
[ 12.229223] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 350!=351. Skipped
[ 12.230515] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 351!=352. Skipped
[ 12.230535] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 351!=352. Skipped
[ 12.251584] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 352!=353. Skipped
[ 12.261873] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 353!=354. Skipped
[ 12.261899] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 353!=354. Skipped
[ 12.273146] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 354!=355. Skipped
[ 12.273168] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 354!=355. Skipped
[ 12.282315] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 354!=355. Skipped
[ 12.283460] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 355!=356. Skipped
[ 12.285524] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 355!=356. Skipped
[ 12.293511] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 357!=358. Skipped
[ 12.309557] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 358!=359. Skipped
[ 12.309583] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 358!=359. Skipped
[ 12.321566] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 359!=360. Skipped
[ 12.323856] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 360!=361. Skipped
[ 12.352782] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 362!=363. Skipped
[ 12.352809] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 362!=363. Skipped
[ 12.363142] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 363!=364. Skipped
[ 12.363167] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 363!=364. Skipped
[ 12.367601] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 364!=365. Skipped
[ 12.374489] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 365!=366. Skipped
add dmesgs:
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.194-rt94+gafe96d2ae0a7 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Tue Nov 28 14:59:04 UTC 2023
[ 0.000000] Machine model: NXP S32G399A-RDB3
[ 0.000000] Xen 4.17 support found
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000083200000, size 3 MiB
[ 0.000000] OF: reserved mem: initialized node pfebufs@83200000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000034400000-0x00000000ff9fffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000034400000-0x000000003449ffff]
[ 0.000000] node 0: [mem 0x0000000034520000-0x00000000345fffff]
[ 0.000000] node 0: [mem 0x0000000083200000-0x00000000835dffff]
[ 0.000000] node 0: [mem 0x00000000835e0000-0x000000008360ffff]
[ 0.000000] node 0: [mem 0x0000000084000000-0x00000000843fffff]
[ 0.000000] node 0: [mem 0x0000000090000000-0x00000000bfffffff]
[ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000c07fffff]
[ 0.000000] node 0: [mem 0x00000000d0000000-0x00000000d03fffff]
[ 0.000000] node 0: [mem 0x00000000e0000000-0x00000000efffffff]
[ 0.000000] node 0: [mem 0x00000000fe200000-0x00000000ff9fffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000034400000-0x00000000ff9fffff]
[ 0.000000] On node 0 totalpages: 273808
[ 0.000000] DMA zone: 4279 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 273808 pages, LIFO batch:63
[ 0.000000] On node 0, zone DMA: 496 pages in unavailable ranges
[ 0.000000] cma: Reserved 256 MiB at 0x00000000b0000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 17 pages/cpu s32536 r8192 d28904 u69632
[ 0.000000] pcpu-alloc: s32536 r8192 d28904 u69632 alloc=17*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [0] 4 [0] 5 [0] 6 [0] 7
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, 1530923, or 1530924
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 269529
[ 0.000000] Kernel command line: console=ttyLF0,115200 earlycon=xen earlyprintk=xen root=/dev/mmcblk0p2 rootwait rw clk_ignore_unused
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 716184K/1095232K available (9470K kernel code, 708K rwdata, 3084K rodata, 1472K init, 270K bss, 116904K reserved, 262144K cma-reserved)
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: 544 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000050900000
[ 0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
[ 0.000557] Console: colour dummy device 80x25
[ 0.000588] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
[ 0.000599] pid_max: default: 32768 minimum: 301
[ 0.000739] LSM: Security Framework initializing
[ 0.000813] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.000827] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.002648] xen:grant_table: Grant tables using version 1 layout
[ 0.002671] Grant table initialized
[ 0.002722] xen:events: Using FIFO-based ABI
[ 0.002751] Xen: initializing cpu0
[ 0.002866] rcu: Hierarchical SRCU implementation.
[ 0.003464] smp: Bringing up secondary CPUs ...
[ 0.004014] Detected VIPT I-cache on CPU1
[ 0.004048] GICv3: CPU1: found redistributor 1 region 0:0x0000000050920000
[ 0.010445] Xen: initializing cpu1
[ 0.010493] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.011095] Detected VIPT I-cache on CPU2
[ 0.011118] GICv3: CPU2: found redistributor 2 region 0:0x0000000050940000
[ 0.017499] Xen: initializing cpu2
[ 0.017538] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.018093] Detected VIPT I-cache on CPU3
[ 0.018115] GICv3: CPU3: found redistributor 3 region 0:0x0000000050960000
[ 0.024495] Xen: initializing cpu3
[ 0.024533] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.025126] Detected VIPT I-cache on CPU4
[ 0.025162] GICv3: CPU4: found redistributor 4 region 0:0x0000000050980000
[ 0.031554] Xen: initializing cpu4
[ 0.031602] CPU4: Booted secondary processor 0x0000000004 [0x410fd034]
[ 0.032197] Detected VIPT I-cache on CPU5
[ 0.032224] GICv3: CPU5: found redistributor 5 region 0:0x00000000509a0000
[ 0.038604] Xen: initializing cpu5
[ 0.038643] CPU5: Booted secondary processor 0x0000000005 [0x410fd034]
[ 0.039244] Detected VIPT I-cache on CPU6
[ 0.039273] GICv3: CPU6: found redistributor 6 region 0:0x00000000509c0000
[ 0.045652] Xen: initializing cpu6
[ 0.045692] CPU6: Booted secondary processor 0x0000000006 [0x410fd034]
[ 0.046271] Detected VIPT I-cache on CPU7
[ 0.046303] GICv3: CPU7: found redistributor 7 region 0:0x00000000509e0000
[ 0.052682] Xen: initializing cpu7
[ 0.052723] CPU7: Booted secondary processor 0x0000000007 [0x410fd034]
[ 0.052851] smp: Brought up 1 node, 8 CPUs
[ 0.052857] SMP: Total of 8 processors activated.
[ 0.052862] CPU features: detected: 32-bit EL0 Support
[ 0.052866] CPU features: detected: CRC32 instructions
[ 0.061147] CPU: All CPU(s) started at EL1
[ 0.061221] alternatives: patching kernel code
[ 0.061981] devtmpfs: initialized
[ 0.068166] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.068211] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.074967] pinctrl core: initialized pinctrl subsystem
[ 0.075832] NET: Registered protocol family 16
[ 0.078039] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.078143] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.078262] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.079000] thermal_sys: Registered thermal governor 'step_wise'
[ 0.079387] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.079859] ASID allocator initialised with 65536 entries
[ 0.079930] xen:swiotlb_xen: Warning: only able to allocate 4 MB for software IO TLB
[ 0.080704] software IO TLB: mapped [mem 0x0000000091c00000-0x0000000092000000] (4MB)
[ 0.080801] Serial: AMBA PL011 UART driver
[ 0.081502] arm-scmi firmware:scmi: SCMI Notifications - Core Enabled.
[ 0.081564] arm-scmi firmware:scmi: SCMI Protocol v2.0 'NXP:S32G399A' Firmware version 0x0
[ 0.103466] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.103476] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.103480] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.103484] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.113307] xen:balloon: Initialising balloon driver
[ 0.113736] vgaarb: loaded
[ 0.113964] SCSI subsystem initialized
[ 0.114093] usbcore: registered new interface driver usbfs
[ 0.114120] usbcore: registered new interface driver hub
[ 0.114148] usbcore: registered new device driver usb
[ 0.114534] pps_core: LinuxPPS API ver. 1 registered
[ 0.114537] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.114549] PTP clock support registered
[ 0.115611] clocksource: Switched to clocksource arch_sys_counter
[ 0.122509] NET: Registered protocol family 2
[ 0.122647] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.123703] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.123773] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.123879] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.124149] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.124258] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.124299] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.124470] NET: Registered protocol family 1
[ 0.124982] RPC: Registered named UNIX socket transport module.
[ 0.124986] RPC: Registered udp transport module.
[ 0.124988] RPC: Registered tcp transport module.
[ 0.124990] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.124999] PCI: CLS 0 bytes, default 64
[ 0.126742] Initialise system trusted keyrings
[ 0.126912] workingset: timestamp_bits=46 max_order=18 bucket_order=0
[ 0.127997] fuse: init (API version 7.32)
[ 0.128206] NET: Registered protocol family 38
[ 0.128217] Key type asymmetric registered
[ 0.128221] Asymmetric key parser 'x509' registered
[ 0.128246] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.128401] io scheduler mq-deadline registered
[ 0.128406] io scheduler kyber registered
[ 0.130027] s32g-siul2-pinctrl 4009c240.siul2-pinctrl: initialized s32 pinctrl driver
[ 0.131011] gpio-345 (sja1110-rst-phy-t1): hogged as output/low
[ 0.131031] gpio-402 (sja1110-rst-core): hogged as output/low
[ 0.132470] xen:xen_evtchn: Event-channel device installed
[ 0.134085] serial: Freescale linflex driver
[ 0.134363] 401c8000.serial: ttyLF0 at MMIO 0x401c8000 (irq = 33, base_baud = 7812500) is a FSL_LINFLEX
[ 0.134413] printk: console [ttyLF0] enabled
[ 0.134866] 401cc000.serial: ttyLF1 at MMIO 0x401cc000 (irq = 34, base_baud = 7812500) is a FSL_LINFLEX
[ 0.135217] 402bc000.serial: ttyLF2 at MMIO 0x402bc000 (irq = 54, base_baud = 7812500) is a FSL_LINFLEX
[ 0.135883] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 0.136460] fsl_fccu 4030c000.fccu: FCCU status is 0 (normal)
[ 0.138106] sja1110-sw@1 enforce active low on chipselect handle
[ 0.139764] spi-nor spi6.0: mx25uw51245g (65536 Kbytes)
[ 0.140321] 7 fixed-partitions partitions found on MTD device 0.spi
[ 0.140326] Creating 7 MTD partitions on "0.spi":
[ 0.140333] 0x000000000000-0x000004000000 : "Flash-Image"
[ 0.140651] 0x000000000000-0x000000280000 : "FIP"
[ 0.140901] 0x000000280000-0x000000290000 : "U-Boot-Env"
[ 0.141154] 0x000000290000-0x000001160000 : "Kernel"
[ 0.141406] 0x000001160000-0x000001190000 : "DTB"
[ 0.141656] 0x000001190000-0x0000030a0000 : "Rootfs"
[ 0.141907] 0x0000030a0000-0x000004000000 : "PFE-Firmware"
[ 0.143220] vcan: Virtual CAN interface driver
[ 0.143225] slcan: serial line CAN interface driver
[ 0.143227] slcan: 10 dynamic interface channels.
[ 0.143232] CAN device driver interface
[ 0.143946] flexcan 401b4000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
[ 0.143953] flexcan 401b4000.flexcan: 25
[ 0.143957] flexcan 401b4000.flexcan: 26
[ 0.143961] flexcan 401b4000.flexcan: 27
[ 0.143965] flexcan 401b4000.flexcan: 28
[ 0.143970] flexcan 401b4000.flexcan: )
[ 0.144475] flexcan 401be000.flexcan: device registered (reg_base=(____ptrval____), irq(s):
[ 0.144480] flexcan 401be000.flexcan: 29
[ 0.144484] flexcan 401be000.flexcan: 30
[ 0.144488] flexcan 401be000.flexcan: 31
[ 0.144493] flexcan 401be000.flexcan: 32
[ 0.144497] flexcan 401be000.flexcan: )
[ 0.144752] e100: Intel(R) PRO/100 Network Driver
[ 0.144756] e100: Copyright(c) 1999-2006 Intel Corporation
[ 0.144789] e1000: Intel(R) PRO/1000 Network Driver
[ 0.144791] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.144819] e1000e: Intel(R) PRO/1000 Network Driver
[ 0.144821] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.144846] igb: Intel(R) Gigabit Ethernet Network Driver
[ 0.144849] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 0.145223] s32cc-dwmac 4033c000.ethernet: IRQ eth_wake_irq not found
[ 0.145228] s32cc-dwmac 4033c000.ethernet: IRQ eth_lpi not found
[ 0.145335] s32cc-dwmac 4033c000.ethernet: no reset control found
[ 0.145377] s32cc-dwmac 4033c000.ethernet: phy mode set to RGMII
[ 0.145548] s32cc-dwmac 4033c000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 0.145558] s32cc-dwmac 4033c000.ethernet: DWMAC4/5
[ 0.145566] s32cc-dwmac 4033c000.ethernet: DMA HW capability register supported
[ 0.145571] s32cc-dwmac 4033c000.ethernet: RX Checksum Offload Engine supported
[ 0.145575] s32cc-dwmac 4033c000.ethernet: TX Checksum insertion supported
[ 0.145579] s32cc-dwmac 4033c000.ethernet: Wake-Up On Lan supported
[ 0.145620] s32cc-dwmac 4033c000.ethernet: Enabled workarounds for s32g274a platform
[ 0.145625] s32cc-dwmac 4033c000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 0.145631] s32cc-dwmac 4033c000.ethernet: Enabled Flow TC (entries=8)
[ 0.145641] s32cc-dwmac 4033c000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 0.145647] s32cc-dwmac 4033c000.ethernet: Using 32 bits DMA width
[ 0.150916] hwmon hwmon0: temp1_input not attached to any thermal zone
[ 0.152493] xen_netfront: Initialising Xen virtual ethernet driver
[ 0.153367] hse-uio 40210000.mu0b: standard firmware, version 2.22.0
[ 0.153378] hse-uio 40210000.mu0b: successfully registered device
[ 0.153623] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 0.153628] ehci-pci: EHCI PCI platform driver
[ 0.153839] usbcore: registered new interface driver uas
[ 0.153870] usbcore: registered new interface driver usb-storage
[ 0.155565] s32gen1-rtc 40060000.rtc: registered as rtc0
[ 0.155675] s32gen1-rtc 40060000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 0.155838] i2c /dev entries driver
[ 0.156305] sac58r-wdt 4010c000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.156519] sac58r-wdt 40200000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.156714] sac58r-wdt 40204000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.156910] sac58r-wdt 40208000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.157126] sac58r-wdt 40500000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.157327] sac58r-wdt 40504000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.157517] sac58r-wdt 40508000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.157713] sac58r-wdt 4050c000.watchdog: SAC58R/S32GEN1 Watchdog Timer Registered. timeout=30s (nowayout=0)
[ 0.157930] sdhci: Secure Digital Host Controller Interface driver
[ 0.157933] sdhci: Copyright(c) Pierre Ossman
[ 0.157935] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.158594] usbcore: registered new interface driver usbhid
[ 0.158597] usbhid: USB HID core driver
[ 0.158920] mmc0: CQHCI version 5.10
[ 0.170033] s32-adc 401f8000.adc: Device initialized successfully.
[ 0.175928] s32-adc 402e8000.adc: Device initialized successfully.
[ 0.176097] nxp_s32_ddr_perf 403e0000.ddr-perf: probing device
[ 0.176367] nxp_s32_ddr_perf 403e0000.ddr-perf: device initialized successfully
[ 0.176630] s32-siul2-nvmem 4009c000.nvram: initialize s32 siul2 nvmem driver
[ 0.176743] s32-siul2-nvmem 44010000.nvram: initialize s32 siul2 nvmem driver
[ 0.176919] optee: probing for conduit method.
[ 0.176964] optee: revision 3.18
[ 0.177243] optee: dynamic shared memory is enabled
[ 0.177752] optee: initialized driver
[ 0.178484] NET: Registered protocol family 10
[ 0.179329] Segment Routing with IPv6
[ 0.179395] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 0.179761] NET: Registered protocol family 17
[ 0.179803] Bridge firewalling registered
[ 0.179943] can: controller area network core
[ 0.179973] NET: Registered protocol family 29
[ 0.179978] can: raw protocol
[ 0.179983] can: broadcast manager protocol
[ 0.179990] can: netlink gateway - max_hops=1
[ 0.180131] 8021q: 802.1Q VLAN Support v1.8
[ 0.180389] printk: console [ttyLF0]: printing thread started
[ 0.180424] Loading compiled-in X.509 certificates
[ 0.187124] i2c i2c-0: using pinctrl states for GPIO recovery
[ 0.187191] i2c i2c-0: using generic GPIOs for recovery
[ 0.187375] pca953x 0-0022: using AI
[ 0.195887] rtc-pcf85063 0-0051: registered as rtc1
[ 0.195918] i2c i2c-0: IMX I2C adapter registered
[ 0.195960] i2c i2c-0: using dma0chan4 (tx) and dma0chan5 (rx) for DMA transfers
[ 0.196514] i2c i2c-2: using pinctrl states for GPIO recovery
[ 0.196550] i2c i2c-2: using generic GPIOs for recovery
[ 0.196637] i2c i2c-2: IMX I2C adapter registered
[ 0.196675] i2c i2c-2: using dma1chan18 (tx) and dma1chan19 (rx) for DMA transfers
[ 0.197200] i2c i2c-4: using pinctrl states for GPIO recovery
[ 0.197237] i2c i2c-4: using generic GPIOs for recovery
[ 0.198864] ina2xx 4-0040: power monitor ina231 (Rshunt = 1000 uOhm)
[ 0.198891] i2c i2c-4: IMX I2C adapter registered
[ 0.198920] i2c i2c-4: using dma1chan20 (tx) and dma1chan21 (rx) for DMA transfers
[ 0.199421] phy-s32gen1-serdes 40480000.serdes: Using mode 0 for SerDes subsystem
[ 0.199779] phy-s32gen1-serdes 44180000.serdes: Using mode 3 for SerDes subsystem
[ 0.204010] mmc0: SDHCI controller on 402f0000.mmc [402f0000.mmc] using ADMA
[ 0.226629] phy-s32gen1-serdes 44180000.serdes: Unstable RX detected on XPCS1
[ 0.226649] phy-s32gen1-serdes 44180000.serdes: Unstable RX detected on XPCS0
[ 0.226831] s32gen1-pcie 40400000.pcie: Configured as RootComplex
[ 0.226952] s32gen1-pcie 40400000.pcie: Allocated line 0 for interrupt 65 (msi)
[ 0.254192] mmc0: new ultra high speed SDR104 SDXC card at address 59b4
[ 0.254766] mmcblk0: mmc0:59b4 SD64G 59.4 GiB
[ 0.256708] mmcblk0: p1 p2 p3 p4 < >
[ 1.227965] s32gen1-pcie 40400000.pcie: Failed to stabilize PHY link
[ 1.227972] s32gen1-pcie 40400000.pcie: Configuring as RootComplex
[ 1.227983] s32gen1-pcie 40400000.pcie: host bridge /soc/pcie@40400000 ranges:
[ 1.228013] s32gen1-pcie 40400000.pcie: IO 0x5ffffe0000..0x5ffffeffff -> 0x0000000000
[ 1.228031] s32gen1-pcie 40400000.pcie: MEM 0x5800000000..0x5ffffdffff -> 0x0000000000
[ 2.228417] s32gen1-pcie 40400000.pcie: Phy link never came up
[ 2.228504] s32gen1-pcie 40400000.pcie: PCI host bridge to bus 0000:00
[ 2.228511] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.228520] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 2.228527] pci_bus 0000:00: root bus resource [mem 0x5800000000-0x5ffffdffff] (bus address [0x00000000-0x7fffdffff])
[ 2.228575] pci 0000:00:00.0: [1957:4300] type 01 class 0x060400
[ 2.228598] pci 0000:00:00.0: reg 0x10: [mem 0x5800000000-0x58000fffff]
[ 2.228619] pci 0000:00:00.0: reg 0x38: [mem 0x5800000000-0x580000ffff pref]
[ 2.228712] pci 0000:00:00.0: supports D1
[ 2.228717] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
[ 2.240943] pci 0000:00:00.0: Failed to add - passthrough or MSI/MSI-X might fail!
[ 2.245393] pci 0000:00:00.0: BAR 0: assigned [mem 0x5800000000-0x58000fffff]
[ 2.245406] pci 0000:00:00.0: BAR 6: assigned [mem 0x5800100000-0x580010ffff pref]
[ 2.245414] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 2.245680] pcieport 0000:00:00.0: PME: Signaling with IRQ 81
[ 2.246690] imx_usb 44064000.usb: No over current polarity defined
[ 2.247256] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 2.247407] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 2.263627] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 2.263761] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 2.263768] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.263775] usb usb1: Product: EHCI Host Controller
[ 2.263779] usb usb1: Manufacturer: Linux 5.10.194-rt94+gafe96d2ae0a7 ehci_hcd
[ 2.263785] usb usb1: SerialNumber: ci_hdrc.0
[ 2.264125] hub 1-0:1.0: USB hub found
[ 2.264148] hub 1-0:1.0: 1 port detected
[ 2.265217] clk: Not disabling unused clocks
[ 2.363235] EXT4-fs (mmcblk0p2): recovery complete
[ 2.365527] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.365574] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.366316] devtmpfs: mounted
[ 2.366842] Freeing unused kernel memory: 1472K
[ 2.443668] Run /sbin/init as init process
[ 2.443673] with arguments:
[ 2.443674] /sbin/init
[ 2.443676] with environment:
[ 2.443678] HOME=/
[ 2.443680] TERM=linux
[ 2.443681] earlyprintk=xen
[ 2.719986] udevd[176]: starting version 3.2.10
[ 2.727442] random: udevd: uninitialized urandom read (16 bytes read)
[ 2.728304] random: udevd: uninitialized urandom read (16 bytes read)
[ 2.728345] random: udevd: uninitialized urandom read (16 bytes read)
[ 2.744739] udevd[177]: starting eudev-3.2.10
[ 2.825831] hse 40211000.mu1b: standard firmware, version 0.0.0
[ 2.825852] hse 40211000.mu1b: volatile configuration, publish SYS_IMAGE
[ 2.826273] hse 40211000.mu1b: registered algs sha1,hmac(sha1)
[ 2.826614] hse 40211000.mu1b: registered algs sha224,hmac(sha224)
[ 2.826992] hse 40211000.mu1b: registered algs sha256,hmac(sha256)
[ 2.827362] hse 40211000.mu1b: registered algs sha384,hmac(sha384)
[ 2.827772] hse 40211000.mu1b: registered algs sha512,hmac(sha512)
[ 2.827915] hse 40211000.mu1b: registered alg ctr(aes)
[ 2.828125] hse 40211000.mu1b: registered alg cbc(aes)
[ 2.828277] hse 40211000.mu1b: registered alg ecb(aes)
[ 2.828450] hse 40211000.mu1b: registered alg cfb(aes)
[ 2.828625] hse 40211000.mu1b: registered alg ofb(aes)
[ 2.828791] hse 40211000.mu1b: registered alg gcm(aes)
[ 2.828942] hse 40211000.mu1b: registered hwrng-hse
[ 2.828947] hse 40211000.mu1b: device ready, status 0x6F20
[ 2.829897] pfeng_slave: loading out-of-tree module taints kernel.
[ 2.840512] pfeng-slave 46000000.pfe_slave: PFEng ethernet driver loading ...
[ 2.840529] pfeng-slave 46000000.pfe_slave: Version: 1.6.0
[ 2.840534] pfeng-slave 46000000.pfe_slave: Driver commit hash: M4_DRIVER_COMMIT_HASH
[ 2.840538] pfeng-slave 46000000.pfe_slave: Multi instance support: SLAVE/mdetect=on
[ 2.840542] pfeng-slave 46000000.pfe_slave: Compiled by: 11.4.0
[ 2.841278] pfeng-slave 46000000.pfe_slave: Wait for PFE controller UP ...
[ 2.841298] pfeng-slave 46000000.pfe_slave: PFE controller UP detected
[ 2.841305] pfeng-slave 46000000.pfe_slave: Cbus addr 0x46000000 size 0x1000000
[ 2.841314] pfeng-slave 46000000.pfe_slave: IHC channel: 3
[ 2.841319] pfeng-slave 46000000.pfe_slave: MASTER IHC channel: 0
[ 2.841335] pfeng-slave 46000000.pfe_slave: netif name: pfe0sl
[ 2.841342] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:00
[ 2.841351] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) linked phyif: 0
[ 2.841357] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) mode: std
[ 2.841391] pfeng-slave 46000000.pfe_slave: netif(pfe0sl) HIFs: count 1 map 08
[ 2.841402] pfeng-slave 46000000.pfe_slave: netif name: pfe1sl
[ 2.841408] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:01
[ 2.841414] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) linked phyif: 1
[ 2.841419] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) mode: std
[ 2.841423] pfeng-slave 46000000.pfe_slave: netif(pfe1sl) HIFs: count 1 map 08
[ 2.841432] pfeng-slave 46000000.pfe_slave: netif name: pfe2sl
[ 2.841437] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:02
[ 2.841443] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) linked phyif: 2
[ 2.841448] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) mode: std
[ 2.841453] pfeng-slave 46000000.pfe_slave: netif(pfe2sl) HIFs: count 1 map 08
[ 2.841462] pfeng-slave 46000000.pfe_slave: netif name: aux0sl
[ 2.841467] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:80
[ 2.841472] pfeng-slave 46000000.pfe_slave: netif(aux0sl) no linked phyif in AUX mode
[ 2.841476] pfeng-slave 46000000.pfe_slave: netif(aux0sl) mode: aux
[ 2.841490] pfeng-slave 46000000.pfe_slave: netif(aux0sl) HIFs: count 1 map 08
[ 2.841499] pfeng-slave 46000000.pfe_slave: netif name: hif0sl
[ 2.841504] pfeng-slave 46000000.pfe_slave: DT mac addr: 00:04:9f:be:ff:f0
[ 2.841511] pfeng-slave 46000000.pfe_slave: netif(hif0sl) linked phyif: 6
[ 2.841516] pfeng-slave 46000000.pfe_slave: netif(hif0sl) mode: std
[ 2.841521] pfeng-slave 46000000.pfe_slave: netif(hif0sl) HIFs: count 1 map 08
[ 2.841526] pfeng-slave 46000000.pfe_slave: HIF channels mask: 0x0008
[ 2.841566] pfeng-slave 46000000.pfe_slave: PFE port coherency enabled, mask 0x1e
[ 2.841620] pfeng-slave 46000000.pfe_slave: assigned reserved memory node pfebufs@83600000
[ 2.841640] pfeng-slave 46000000.pfe_slave: PFE CBUS p0x(____ptrval____) mapped @ v0xffffffc012000000
[ 2.841649] pfeng-slave 46000000.pfe_slave: Wait for Master UP ...
[ 2.841661] pfeng-slave 46000000.pfe_slave: Detected Master UP
[ 2.841681] pfeng-slave 46000000.pfe_slave: HIF3 is in clean state
[ 2.841885] pfeng-slave 46000000.pfe_slave: HIF0 not configured, skipped
[ 2.841893] pfeng-slave 46000000.pfe_slave: HIF1 not configured, skipped
[ 2.841897] pfeng-slave 46000000.pfe_slave: HIF2 not configured, skipped
[ 2.842233] pfeng-slave 46000000.pfe_slave: HIF3 enabled
[ 2.842243] pfeng-slave 46000000.pfe_slave: HIF3 started
[ 2.842248] pfeng-slave 46000000.pfe_slave: IDEX-slave @ master-interface 6
[ 2.842259] pfeng-slave 46000000.pfe_slave: IHC client registered
[ 2.846334] pfeng-slave 46000000.pfe_slave: IDEX: v2 protocol used, Resend:count=10,delay=100ms
[ 2.846350] pfeng-slave 46000000.pfe_slave: IDEX RPC installed on HIF3
[ 2.846389] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Subscribe to HIF3
[ 2.846421] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Subscribe to HIF3
[ 2.846427] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Host LLTX disabled
[ 2.846451] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Subscribe to HIF3
[ 2.846470] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Subscribe to HIF3
[ 2.846499] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Subscribe to HIF3
[ 2.846507] pfeng-slave 46000000.pfe_slave: MDIO bus 0 disabled: Not found in DT
[ 2.846512] pfeng-slave 46000000.pfe_slave: MDIO bus 1 disabled: Not found in DT
[ 2.846518] pfeng-slave 46000000.pfe_slave: MDIO bus 2 disabled: Not found in DT
[ 2.880610] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 5!=6. Skipped
[ 2.885708] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 6!=7. Skipped
[ 2.890843] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 7!=8. Skipped
[ 2.895960] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 8!=9. Skipped
[ 2.929388] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 2.937990] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 14!=15. Skipped
[ 2.946332] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): Enable HIF3
[ 2.983806] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 21!=22. Skipped
[ 2.984741] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): receive traffic matching its MAC address
[ 2.984750] pfeng-slave 46000000.pfe_slave pfe0sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:00
[ 2.989624] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 22!=23. Skipped
[ 2.996470] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 23!=24. Skipped
[ 3.030740] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.036191] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 30!=31. Skipped
[ 3.036976] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.043915] pfeng-slave 46000000.pfe_slave pfe0sl: registered
[ 3.043950] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Host LLTX disabled
[ 3.088897] wlan: Loading MWLAN driver
[ 3.089562] wlan: Driver loaded successfully
[ 3.089751] wlan: Register to Bus Driver...
[ 3.089844] wlan: Register to Bus Driver Done
[ 3.095190] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 38!=39. Skipped
[ 3.103343] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): Enable HIF3
[ 3.109549] sja1110 spi5.0: probing uc
[ 3.109704] sja1110 spi5.1: probing switch
[ 3.110001] sja1110 spi5.1: Could not get GPIO from device tree
[ 3.110016] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[ 3.110511] sja1110 spi5.1: [sja1110_init_hw] loaded fw 'sja1110_switch.bin'
[ 3.110633] sja1110 spi5.1: [sja1110_pre_switch_upload] Found switch config of size 2236
[ 3.110817] sja1110 spi5.1: Uploading config...
[ 3.116455] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 42!=43. Skipped
[ 3.122177] random: crng init done
[ 3.122185] random: 4 urandom warning(s) missed due to ratelimiting
[ 3.122472] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): receive traffic matching its MAC address
[ 3.122480] pfeng-slave 46000000.pfe_slave pfe1sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:01
[ 3.150819] sja1110 spi5.1: Successfully configured!
[ 3.150845] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[ 3.155208] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'
[ 3.155215] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 320280
[ 3.155304] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid
[ 3.155379] sja1110 spi5.0: [sja1110_pre_uc_upload] \xc2\xb5C not ready for download (Status=0x31)
[ 3.155666] sja1110 spi5.0: Uploading firmware...
[ 3.187650] pfeng-slave 46000000.pfe_slave pfe1sl: registered
[ 3.187672] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Host LLTX disabled
[ 3.198823] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 53!=54. Skipped
[ 3.229905] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 58!=59. Skipped
[ 3.236914] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 59!=60. Skipped
[ 3.244064] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): Enable HIF3
[ 3.267230] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): receive traffic matching its MAC address
[ 3.267247] pfeng-slave 46000000.pfe_slave pfe2sl (uninitialized): setting MAC addr: 00:04:9f:be:ff:02
[ 3.313623] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 70!=71. Skipped
[ 3.339562] pfeng-slave 46000000.pfe_slave pfe2sl: registered
[ 3.339598] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Host LLTX disabled
[ 3.347534] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 73!=74. Skipped
[ 3.366104] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 75!=76. Skipped
[ 3.366837] pfeng-slave 46000000.pfe_slave aux0sl (uninitialized): Enable HIF3
[ 3.367317] pfeng-slave 46000000.pfe_slave aux0sl: checksum offload not possible for AUX interface
[ 3.367614] pfeng-slave 46000000.pfe_slave aux0sl: registered
[ 3.367628] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Host LLTX disabled
[ 3.388151] pfeng-slave 46000000.pfe_slave: IDEX: Wrong sequence number in RPC response: 78!=79. Skipped
[ 3.388820] pfeng-slave 46000000.pfe_slave hif0sl (uninitialized): Enable HIF3
[ 3.389585] pfeng-slave 46000000.pfe_slave hif0sl: registered
[ 4.063701] IPv6: ADDRCONF(NETDEV_CHANGE): pfe0sl: link becomes ready
[ 4.248112] sja1110 spi5.0: Upload successfully verified!
[ 4.334725] s32cc-dwmac 4033c000.ethernet eth0: PHY [stmmac-0:01] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[ 4.356308] s32cc-dwmac 4033c000.ethernet eth0: Enabling Safety Features
[ 4.356413] s32cc-dwmac 4033c000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 4.356677] s32cc-dwmac 4033c000.ethernet eth0: registered PTP clock
[ 4.357088] s32cc-dwmac 4033c000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 4.359996] 8021q: adding VLAN 0 to HW filter on device eth0
[ 4.422729] xenbr0: port 1(eth0) entered blocking state
[ 4.422783] xenbr0: port 1(eth0) entered disabled state
[ 4.423148] device eth0 entered promiscuous mode
[ 4.462507] xenbr0: port 1(eth0) entered blocking state
[ 4.462530] xenbr0: port 1(eth0) entered forwarding state
[ 5.087883] xenbr0: port 1(eth0) entered disabled state
[ 6.654700] v2xbr: port 1(vif1.1) entered blocking state
[ 6.654763] v2xbr: port 1(vif1.1) entered disabled state
[ 6.655062] device vif1.1 entered promiscuous mode
[ 6.655545] xenbr0: port 2(vif1.0) entered blocking state
[ 6.655554] xenbr0: port 2(vif1.0) entered disabled state
[ 6.655779] device vif1.0 entered promiscuous mode
[ 6.944183] xen-blkback: backend/vbd/1/51712: using 2 queues, protocol 1 (arm-abi) persistent grants
[ 6.988627] vif vif-1-0 vif1.0: Guest Rx ready
[ 6.988701] IPv6: ADDRCONF(NETDEV_CHANGE): vif1.0: link becomes ready
[ 6.988933] xenbr0: port 2(vif1.0) entered blocking state
[ 6.988944] xenbr0: port 2(vif1.0) entered forwarding state
[ 6.999234] vif vif-1-1 vif1.1: Guest Rx ready
[ 6.999321] IPv6: ADDRCONF(NETDEV_CHANGE): vif1.1: link becomes ready
[ 6.999560] v2xbr: port 1(vif1.1) entered blocking state
[ 6.999573] v2xbr: port 1(vif1.1) entered forwarding state
[ 12.845625] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready
[ 13.855654] IPv6: ADDRCONF(NETDEV_CHANGE): can1: link becomes ready