TJA1057GTK/3 & TJA1043TK Failure Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1057GTK/3 & TJA1043TK Failure Detection

357 Views
Vishal25
Contributor I

Hi Team,

 

We are using TJA1057GTK/3 and TJA1043TK in our design.

We would like to know if the CAN transceiver is capable of the following

1.Informing SOC when a Invalid Data (Sended) failure is detected on CAN_H and CAN_L in less than 400ms

2. To inform SOC when a Bus OFF failure is detected on CAN wire CAN_H and CAN_L in less than 400ms

3. To inform SOC when a Missing Frame failure is detected on CAN wire CAN_H and CAN_L in less than 400ms

 

If it is capable , how this can be verified/checked.

If not is there any provision that we could implement this feature?

 

Regards,

Vishal.A

0 Kudos
Reply
1 Reply

342 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please read out the AH1014 page 54-58 for your concern questions.

Application Hints (nxp.com)

0 Kudos
Reply