S32g274 RDB2开发板uboot使用PFE MAC0报错加载PFE固件错误

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32g274 RDB2开发板uboot使用PFE MAC0报错加载PFE固件错误

151 Views
sdx111
Contributor I

您好,

我使用的是BSP35.0,yocto编译,PFE固件版本1.5.0。

我想要在uboot阶段使用开发板的PFEMAC0网口,但是给EMMC下完fip.s32-sdcard文件后会提示PFE固件加载失败。不过如果我用整个包含文件系统的程序在uboot启动时就不会提示这个错误。

如果我想要把fip.s32-sdcard文件下载到EMMC后就能应用PFEMAC0网口应该怎么操作?也就是仅有uboot的情况下也能成功加载PFE固件。

0 Kudos
2 Replies

113 Views
chenyin_h
NXP Employee
NXP Employee

您好, 感谢提出问题。

您可以尝试一下以下办法:

1. 首先写入整个包含文件系统的image到SD/MMC,如您所说,应该是可以正常加载PFE固件的。

2. 然后再写入fip.s32-sdcard这个文件,可以参考如下命令:

sudo dd if=fip.s32-sdcard of=/dev/sdx bs=1 skip=4096 seek=4096 && sync

 

Best Regards

Chenyin

0 Kudos

112 Views
sdx111
Contributor I
我是用flash tool工具直接把fip.s32-sdcard刷到EMMC的,这个现象应该是找不到PFE固件所在的位置了吧,如果我想要看编译的时候固件被放到EMMC哪个位置的话,应该怎么看?
0 Kudos