S32G SJA1110 CB(frer) enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G SJA1110 CB(frer) enable

623 Views
wangbaozeng90
Contributor II

wangbaozeng90_0-1657760442459.png

The test topology is shown in the figure.

The data received from the P6 port has the same data at the P8 and P10 ports after passing through sja1110.

According to the following configuration, the CB function is not effective.

Table 1168. General parameters table.
SEQNUM_GREATER
CB_EN
Table 1138. CB Sequence Generation/Individual Recovery table
RTAGOFFSET(10)
RTAGOFFSET(9)
RTAGOFFSET(8)
RTAGOFFSET(7)
RTAGOFFSET(6)
RTAGOFFSET(5)
RTAGOFFSET(4)
RTAGOFFSET(3)
RTAGOFFSET(2)
RTAGOFFSET(1)
RTAGOFFSET(0)
REPLACE_PORTS
TAG_PORTS
GENSEQNUM
Table 1141. CB Stream Out table
STREAMOUTID
PORTID
Table 1159. Deep packet inspection parameters table
MAXDEEP
PVIDFORUNTAGGED
Table 1160. Deep packet inspection table: 16 bytes deep
KEY[0]
MASK[0]
VALIDSMALLER48
VALIDSMALLER64
VALIDSMALLER80
VALIDSMALLER96
VALIDSMALLER112
VALIDSMALLER128
DSTPORTS
CB_EN
CB_SID_IN

In addition, where is the stream splitting function configured?

Tags (1)
0 Kudos
Reply
0 Replies