S32G IPCF runs in an endless loop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G IPCF runs in an endless loop

758 Views
jack_huang1
Contributor III

Dear,

The S32G2 platform is based on IPCF4.8.0.

Q1:  After the configuration is interrupted 19, the program keeps entering the ISR(Ipc_Hard_irq_handle) function after running. See Appendix 1 for the implementation of the function.       

Q2: IPCF reverted to version 4.6.0 with an unhandleirq error, and then IPCF changed from 4.6.0 to 4.8.0 with the same error screenshot as attached 2.

 Thank you!

 Best Regards!

0 Kudos
Reply
2 Replies

741 Views
nxf92355
NXP Employee
NXP Employee

Hi Jack

 

Hope you are doing well

Can you some brief on "After the configuration is interrupted 19" ?

Can you tell which document you are talking "Appendix 1 for the implementation of the function" ?

 

Regards ,

Tushar

 

0 Kudos
Reply

701 Views
jack_huang1
Contributor III

Dear Tushar:

          It's solved now, because our system versions don't match it.

 

         Thank you!

          Best Regards!

0 Kudos
Reply