Network error on s32g QNX7.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Network error on s32g QNX7.1

Jump to solution
228 Views
lewis123
Contributor II

Dear NXP,

 

I am running QNX7.1 on S32G-VNP-RDB2, but there are problems with the network.

The NIC dwc0 is identified after the system starts, I configured a valid ip for it.
But it can not ping other machines(return info: "ping: sendto: Host is down"), and no machine could ping the board.

Could you please suggest, is there any other work that needs to be done here.

Thank you for your support.

Tags (1)
0 Kudos
Reply
1 Solution
207 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

View solution in original post

0 Kudos
Reply
1 Reply
208 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

0 Kudos
Reply