Network error on s32g QNX7.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Network error on s32g QNX7.1

ソリューションへジャンプ
100件の閲覧回数
lewis123
Contributor II

Dear NXP,

 

I am running QNX7.1 on S32G-VNP-RDB2, but there are problems with the network.

The NIC dwc0 is identified after the system starts, I configured a valid ip for it.
But it can not ping other machines(return info: "ping: sendto: Host is down"), and no machine could ping the board.

Could you please suggest, is there any other work that needs to be done here.

Thank you for your support.

タグ(1)
0 件の賞賛
1 解決策
79件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

元の投稿で解決策を見る

0 件の賞賛
1 返信
80件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Check with QNX since this works with the NXP BSP,

Regards

0 件の賞賛