IPCF sample application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IPCF sample application

1,546 次查看
SriramVenkat
Contributor II

Hello,

I tried compiling the IPCF application framework given for NXP S32 RTD running on Cortex-M7 core of NXP S32 platform. The application was builded for bare-metal. To access the shared memory whether any other framework is required other than the IPCF_4.6.0_D2205.

Also, is there any flashing procedure available for Cortex-M7 core?

0 项奖励
回复
1 回复

1,524 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might be misunderstanding the request. Below will be some comments.

IPCF is available on both the bare-metal application inside the M7 core (with the examples provided under the IPCF package) and linux. Under the IPCF example (the one for M7 core) a "description.txt" is provided, in which detailed steps are provided on how to run the example application.

Also, which RTD/BSP versions are you using?

Please, let us know.

0 项奖励
回复