Added support for GD25LQ128D qspi flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Added support for GD25LQ128D qspi flash

跳至解决方案
113 次查看
shiyiheng
Contributor I

Now I am developing based on BSP34 branch and want to add GD25LQ128D qspi flash support under uboot. The device tree configuration is as follows, but I failed to read JEDEC, and I found that only macronix and micron products are supported based on this branch. What do I need to do if I want to support GD25LQ128D?

shiyiheng_0-1718247116648.png

 

0 项奖励
1 解答
65 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

在原帖中查看解决方案

0 项奖励
1 回复
66 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

0 项奖励