Added support for GD25LQ128D qspi flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Added support for GD25LQ128D qspi flash

ソリューションへジャンプ
114件の閲覧回数
shiyiheng
Contributor I

Now I am developing based on BSP34 branch and want to add GD25LQ128D qspi flash support under uboot. The device tree configuration is as follows, but I failed to read JEDEC, and I found that only macronix and micron products are supported based on this branch. What do I need to do if I want to support GD25LQ128D?

shiyiheng_0-1718247116648.png

 

0 件の賞賛
1 解決策
66件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

元の投稿で解決策を見る

0 件の賞賛
1 返信
67件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

0 件の賞賛