Added support for GD25LQ128D qspi flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Added support for GD25LQ128D qspi flash

Jump to solution
200 Views
shiyiheng
Contributor I

Now I am developing based on BSP34 branch and want to add GD25LQ128D qspi flash support under uboot. The device tree configuration is as follows, but I failed to read JEDEC, and I found that only macronix and micron products are supported based on this branch. What do I need to do if I want to support GD25LQ128D?

shiyiheng_0-1718247116648.png

 

0 Kudos
Reply
1 Solution
152 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

View solution in original post

0 Kudos
Reply
1 Reply
153 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to add you hardware to the device tree and create the drivers is needed it, but the BSP include driver for SPI you must check it.

Regards

0 Kudos
Reply