while creating a new s32ds application project, while selecting tool chain(NXP GCC 9.2 FOR Arm 32-bite bare metal) , following next button and selecting the cores and parameters (SDK IS NOT SHOWING).
Whereas while selecting NXP GCC 6.3 for Arm , SDK options are available(free master_s32k144, s32k144_sdk)
Some issues have been reported with S32K1 support in S32DS v3.5, at this moment we recommend for the S32K1 family use the S32DS v3.4 since it has support for the latest version of SDK (4.0.3) and RTDs (1.0.1) available for the family.
Sorry for the inconvenience.
Thanks, Let me try with the earlier version then.
Also would like to know do I need to install VDK? Also to know where I can install the versions of Synopsys Virtualizer Studio and VDK packages .
Please do share the link for S32 Design Studio for S32 Platform 3.4 Release Notes
You can consult the release notes of S32DS v3.4 at the below link:
S32 Design Studio 3.4 – Windows/Linux -> S32 Design Studio IDE -> Previous tab.
Regarding Synopsys Virtualizer Studio and VDK packages please get in touch with Synopsys for further support in this part.