s32k344 rtd 3.0.0 p07
Can the s32k344 LIN Slave receive both enhanced and classic check data?
I can only choose one of the following ways to receive
void LIN_Slave_Callback (uint8 Instance, const Lpuart_Lin_Ip_StateStructType *LpuartStateStruct)
{
Lpuart_Lin_Ip_PduType LinPdu_rx =
{
.Pid = LpuartStateStruct->CurrentPid,
.Cs = LPUART_LIN_IP_CLASSIC_CS,
.SduPtr = NULL_PTR,
.Drc = LPUART_LIN_IP_FRAMERESPONSE_RX,
.Dl = (uint8)BUFFER_SIZE
};
Lpuart_Lin_Ip_PduType LinPdu_tx =
{
.Pid = LpuartStateStruct->CurrentPid,
.Cs = LPUART_LIN_IP_CLASSIC_CS,
.SduPtr = Slave_TxBuff,
.Drc = LPUART_LIN_IP_FRAMERESPONSE_TX,
.Dl = (uint8)BUFFER_SIZE
};
switch (LpuartStateStruct->CurrentEventId)
{
case LPUART_LIN_IP_RECV_HEADER_OK:
if(LpuartStateStruct->CurrentPid == PID_SLAVE_RECEIVE_DATA)
{
Lpuart_Lin_Ip_SendFrame(Instance, (const Lpuart_Lin_Ip_PduType *)&LinPdu_rx);
}
if(LpuartStateStruct->CurrentPid == PID_MASTER_RECEIVE_DATA)
{
Lpuart_Lin_Ip_SendFrame(Instance, (const Lpuart_Lin_Ip_PduType *)&LinPdu_tx);
}
break;
case LPUART_LIN_IP_SEND_HEADER_OK:
break;
case LPUART_LIN_IP_TX_COMPLETED:
//Lin_MasterRecv_Irq_Flag = 1;
break;
case LPUART_LIN_IP_RX_COMPLETED:
Siul2_Dio_Ip_TogglePins(LED3_BLUE_PORT,1<<LED3_BLUE_PIN);
Lin_SlaveRecv_Irq_Flag = 1;
break;
default:
/* do nothing */
break;
}
}
int main(void)
{
Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);
IntCtrl_Ip_Init(&IntCtrlConfig_0);
Get_Freq = Clock_Ip_GetClockFrequency(CORE_CLK);
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
Lpuart_Lin_Ip_Init(Lpuart_Lin_Ip_Sa_pHwConfigPB_1.Instance, &Lpuart_Lin_Ip_Sa_pHwConfigPB_1);
while(1)
{
if( Lin_SlaveRecv_Irq_Flag ==1) //处理从机接收标志位
{
/*此函数用来查询LIN总线状态 比如总线繁忙,接收完成或失败等。并且当接收成功时,可以把接收到的数据拷贝进接收缓存。*/
do
{
LpuartSlaveStatus = Lpuart_Lin_Ip_GetStatus(Lpuart_Lin_Ip_Sa_pHwConfigPB_1.Instance, (uint8 **)&RecvBuffer);
}
while (LPUART_LIN_IP_STATUS_RX_OK != LpuartSlaveStatus); //查询总线状态并且接收数据
CopyBufferToData(Slave_RxBuff,RecvBuffer,8); //把接受到的数据拷贝进数据缓存
memset(RecvBuffer,0,8*sizeof(uint8));//清除缓存,为下一次接收做准备
LPUART_printf("Lin总线从机接收到的数据 :\r\n");//打印接收数据
for(int i=0; i<8 ;i++)
{
LPUART_printf("data %d : 0x%x\r\n",i,Slave_RxBuff[i]);
}
Lin_SlaveRecv_Irq_Flag =0; //清零标志位,等待下一次接收
}
}
return 0;
}
Hi,
yes, this is possible. You need to have more PDUs defined for this, to have unique Pid with desired checksum type.
BR, Petr