How can i change the package in S32DS and generate code that can compile successfully?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i change the package in S32DS and generate code that can compile successfully?

1,168 Views
timwang
Contributor II

捕获.PNG

When i change the package of the processor MPC5748G and generate code,if i build the project,there are some faults exist like this:

捕获.PNG

How can i use the PE tool to change the pacage of processor and add some other components?

When i add some other components,it also can't compile successfully.

Thanks!

0 Kudos
1 Reply

934 Views
stanish
NXP Employee
NXP Employee

Hi,

there is a document describing switching the package, it should be the same process for S32DS Power.

 https://community.nxp.com/docs/DOC-334936 

S.