Hello,
I am migrating an existing project based on the previous RTD (AR: 4.4.0, SW: 1.0.0) to the latest version (AR: 4.7.0, SW: 2.0.0 ). I am currently using the S32DS v3.5.12.
I have noticed that in the ConfigTools under the section MCAL the Fls driver is renamed/replaced by the Mem_43_INFLS, which should be the proper replacement, right?
When I attempt to build the application an error is thrown pointing at the generated C source file
with the statement
'E_MEM_SERVICE_NOT_AVAIL' undeclared (first use in this function) Mem_43_INFLS.c /my_project/RTD/src line 1013 C/C++ Problem
I have checked the BaseNXP driver documentation (RTD_BASE_UM.pdf) and noticed that the missing C macro is specified at page 151.
Then I checked the StandardTypes.h header file at line 141 but the macro -- as expected -- was missing.
Can you point out what the issue is and if I am missing something.
As a side node, I have found out that the macro is also defined in the MemAcc_GeneralTypes.h, which is not generated in my project right now.
One last thing: I have installed the following RTD package versions:
Best regards,
M_SCH
已解决! 转到解答。
You are right, it is missing in 2.0.0 P03, it is defined in 2.0.0 and 2.0.0 P04.
Regadrs,
Daniel
Hello Daniel,
since I have installed the P03 and P04 RTD (AR: 4.7.0, SW: 2.0.0) package for the S32K1 series and the StandardTypes.h file which is included directly through the RTD installation folder at
which shows the following version of the StandardTypes.h file:
Can you tell me how I can generate the code from the RTD P04 instead of the P03 package version again?
Best regards,
M_SCH
It looks like an issue with the P04 installation.
I also updated to P04 from P03, but I have
S32K1_RTD_2_0_0_P04_D2404_ASR_REL_4_7_REV_0000_20240417
in the very same directory.
Maybe you can reinstall P04 in S32DS Extensions and Updates.
BR, Daniel
Hello,
I have uninstalled the RTD packages P03 and P04 of the latest version (AR: 4.7.0, SW: 2.0.0) and then installed P03 and then P04. Now all C source and header files indicate that they belong to P04 through their file header comment block but now I am missing again drivers such as the Crypto driver that is only available through P03 and both packages cannot coexist.
Can you confirm this on your side as well?
Best regards,
M_SCH
Hello,
as you may recall I have installed the P03 package to make use of the Crypto Driver but at the same time I am missing the macro for the FLS driver that I mentioned in my original post and therefore cannot continue. Can you help me out? Do you have any suggestions?
Best regards
M_SCH
Hello Daniel,
I think you are missing the point. If you read my initial post you see that the C macro E_MEM_SERVICE_NOT_AVAIL is not available in the StandardTypes.h file in the P03 package. So I get errors using the FLS driver. That is why I posted this issue.
Can you confirm this issue on your side?
Best regards
M_SCH