Update S32 Design Studio for Arm to SDK RTM 4.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update S32 Design Studio for Arm to SDK RTM 4.0

1,184 Views
Revinio
Contributor I

Hello,

I try to use the SDK RTM 4.0 in the S32 Design Studio for Arm V2.2 because of the "Processor Expert CAN ISR bug". But I don't manage to include it. For example I removed the SDK 3.0 und installed the SDK 4.0 .exe. The path variable should be added automaticly but it does not. When I try to add the SDK with SDK Management, there is no "sources.xml" to add. In the foldes its named "sources_S32K1xx_SDK.xml". I think that is the reason why i can't add it. If i rename it to "sources.xml" it does not work.

Do you have an idea how to fix this problem?

Thanks

Revinio

 

EDIT:

It seems, that SDK RTM V4.0 is not compatible at the moment with Design Studio for Arm 2.2.

I downloaded Design Studio For S32 Platform 3.3 and now I can use SDK RTM V4.0.

Best Regards

Revinio

 

 

 

 

Labels (1)
1 Reply

1,166 Views
jiri_kral
NXP Employee
NXP Employee

Hi Revinio, 

 

you are right - SDK S32K1XX RTM 4.0.0 is for S32DS v3.3.

 

Jiri  

0 Kudos