S32DSV3.1 debug issue with S32_SDK_RTM_1.0.0 can_pal example use U-MULTILINK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DSV3.1 debug issue with S32_SDK_RTM_1.0.0 can_pal example use U-MULTILINK

Jump to solution
1,704 Views
nxf46962
NXP Employee
NXP Employee

The customer is Deeproute. customer try to use the S32DS 3.1 to debug issue with can_pal example. the  error log:

Error in services launch sequence PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor. Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.

I try to use different example, the result is same.

best regards

deqing.liu

0 Kudos
1 Solution
1,585 Views
nxf46962
NXP Employee
NXP Employee

Hello Jiri,

I solved the isue. I just take off the SD card.

I think you need to upgrade the S32 Design Studio Platform Tools Package and S32V2XX development package.

best regards

deqing.liu

View solution in original post

0 Kudos
3 Replies
1,585 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried your scenario - and ended in the same state. But mine issue is related to some PE Micro issue. It looks that firmware in PE Micro Multilink can't be updated - for some reason: 

pastedImage_1.png

Are you facing the same issue? 

Jiri 

0 Kudos
1,586 Views
nxf46962
NXP Employee
NXP Employee

Hello Jiri,

I solved the isue. I just take off the SD card.

I think you need to upgrade the S32 Design Studio Platform Tools Package and S32V2XX development package.

best regards

deqing.liu

0 Kudos
1,585 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

update doesn't work, but it looks that it is my local (probably network?) issue. Glad to see that you solved your issue. 

Jiri 

0 Kudos