Hi
Except that you set the wrong pin for CAN0_EN in the Pins Tool, everything else is correct (CAN0_EN should be PTC30 instead of PTC28). I can observe that the PTC28\PTC30 becomes high level on S32K344EVB.
Please check your hardware, e.g. pin output is connected correctly to TJA1443.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------