Error to compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error to compiler

2,945 Views
antonkarzanov
Contributor II

Hello.

I have S32DS for ARM Version: 2.0 . I use SAC57D54 and Freertos.

At the end compile my project I have four error .
I know a cause this errors. And I eliminated this cause.
But problems is not solve. All functions is declared and have prototipe. All header files is included.
Help me please.

Tags (3)
4 Replies

2,609 Views
antonkarzanov
Contributor II

OK. I attach my project.

0 Kudos
Reply

2,609 Views
jiri_kral
NXP Employee
NXP Employee

It looks like that you forgot define configLED_TEST preprocessor flag. For linker was implementation of functions mentioned above invisible in that case. I add the flag in the project settings (right click on project name in the project explorer):

pastedImage_1.png

I got some warnings - but project can be compiled successfully.

Jiri

2,609 Views
antonkarzanov
Contributor II

Thank you!

0 Kudos
Reply

2,609 Views
jiri_kral
NXP Employee
NXP Employee

Hi Anton, 

can you share your project? Linker can't find LED_on(), LED_off() and vParTestInitialiseLED() founcions. Is the header file with function declaration visible for your project (in the include paths)? 

Jiri

0 Kudos
Reply