using the CW MCU v11.1 development platform, the PE tool failed to burn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using the CW MCU v11.1 development platform, the PE tool failed to burn

499件の閲覧回数
zhouqicheng
Contributor I

Hello, using the CW MCU v11.1 development platform, the PE tool failed to burn and the circuit board has 5V. The following interface always pops up. How can I solve this problem

0 件の賞賛
1 返信

485件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

if you have a problem with P&E USB Multilink Universal (firmware update), then you should ask P&E support. www.pemicro.com

However.....

I suppose you use Windows 10.

Did it work before?

Have you plugged the cable in correct orientation into the board?

Are you using your own board or an EVB?

 

Best regards,

Ladislav

0 件の賞賛