using the CW MCU v11.1 development platform, the PE tool failed to burn

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using the CW MCU v11.1 development platform, the PE tool failed to burn

512 次查看
zhouqicheng
Contributor I

Hello, using the CW MCU v11.1 development platform, the PE tool failed to burn and the circuit board has 5V. The following interface always pops up. How can I solve this problem

0 项奖励
1 回复

498 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

if you have a problem with P&E USB Multilink Universal (firmware update), then you should ask P&E support. www.pemicro.com

However.....

I suppose you use Windows 10.

Did it work before?

Have you plugged the cable in correct orientation into the board?

Are you using your own board or an EVB?

 

Best regards,

Ladislav

0 项奖励