9S12E - Toggling an external pin on an output compare event

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12E - Toggling an external pin on an output compare event

1,935件の閲覧回数
Beaker
Contributor I

I'm having trouble getting an external pin to toggle on an output compare event.  I've had lots of success using the output compare feature to generate software delays.  I just can't figure out how to get the hardware to automatically toggle the associated IOC pin.
 
I'm using a MC9S12E64 device in a 112 pin package.
I'd like to get PortU.0 / IOC2.4 (pin 32) to toggle on a timer 2 channel 4 output compare event.
 
I put some test code in the Timer 2 channel 4 interrupt routine to toggle an unused pin on port P.  With an oscilloscope I can see that the output compare is working correctly, but the IOC24 pin is not toggling.
 
So far my code looks like this:

Code:

//---------------- Timer 2 ----------------// setups specific to Timer 2 TIM2_TSCR1_TEN = 0;  // inhibit timer 2 during register initializationTIM2_TSCR1_TSWAI = 1;  // timer disabled when CPU is in wait modeTIM2_TSCR1_TSFRZ = 1;  // timer disabled when CPU is in freeze modeTIM2_TSCR1_TFFCA = 0;  // normal flag clearing modeTIM2_TSCR2_TOI = 0;  // disable timer overflow interruptTIM2_TSCR2_TCRE = 0;  // counter reset inhibited and counter free runsTIM2_TSCR2_PR = 4;  // prescaler = bus clock/16 = 20Mhz/16 = 800nsec prescaler clk periodTIM2_TFLG1 = TIM2_TFLG1_C4F_MASK | TIM2_TFLG1_C5F_MASK |       TIM2_TFLG1_C6F_MASK | TIM2_TFLG1_C7F_MASK; // clear capture event flagsMODRR = 0x00;   // timer 2 channels 4,5,6,7 are on PU0,PU1,PU2,PU3 pins// - - - - - - - - - - - - - - - - - - - - - - - -// setups specific to channel 4TIM2_OC7M_OC7M4 = 0;  // no output port assignment on output compareTIM2_OC7D_OC7D4 = 0;  // no output compare 7 mapping to port 4TIM2_TIOS_IOS4 = 1;  // configured as output compareTIM2_TCTL1_OM4 = 0;  // toggle PortU.0 (IOC2.4)TIM2_TCTL1_OL4 = 1;TIM2_TTOV_TOV6 = 0;  // inhibit output compare pin toggle on timer overflowTIM2_TIE_C4I = 0;  // timer interrupt disabled    // The channel 4 initialization will enable this interrupt// - - - - - - - - - - - - - - - - - - - - - - - -// setups specific to Timer 2TIM2_TSCR1_TEN = 1;  // enable timer 2//-----------------------------------------//---------------- Port U ----------------    // set bits 0 and 4-7 as outputs / all others as inputsDDRU = DDRU_DDRU0_MASK | DDRU_DDRU4_MASK | DDRU_DDRU5_MASK |       DDRU_DDRU6_MASK | DDRU_DDRU7_MASK;RDRU = 0x00;   // all outputs drive at full strengthPTU = 0x00;   // set the output pins to their reset state   /****************************************************************************//* initChannel4() - initialize timer 2 channel 4         *//****************************************************************************/void initChannel4(){ PTP_PTP0 = 0;    // set the initial state of the debug pin TIM2_TC4 = TIM2_TCNT + Delay; // set up the first interrupt for 1msec latter  TIM2_TIE_C4I = 1;   // enable the Timer 2 channel 4 interrupt }/********************************************************************************//* time_ch4_isr() - Timer2 Channel 4 Interrupt code      *//********************************************************************************/__interrupt void tim2_ch4_isr(){ if (PTP_PTP0)    // toggle PortP.0 for DEBUG  PTP_PTP0 = 0; else  PTP_PTP0 = 1;  TIM2_TC4 = TIM2_TCNT + Delay; // set up the next interrupt TIM2_TFLG1 = TIM2_TFLG1_C4F_MASK; // clear timer 2 channel 4 interrupt request flag}


Does anyone have any suggestions as to why PortU.0 / ICO2.4 is not toggling?

I also tried creating a project using processor expert and the TimerOut bean and it generated similar code with similar results.

Is there a problem using bit fields to set up some some of the timer registers?  I do set up channels 5 - 7 after channel 4 using bit field defines as well.

Based on the documentation, I'm also slightly confused as to how the OC7M register should be set up.  I tried setting the bits in this register as a test, but got the same results.

Any help would be greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

849件の閲覧回数
Beaker
Contributor I
Nevermind.
I tried my code on another one of our proto boards and the pin toggles just fine.  Apparently, there is something pulling down this pin on my board.
0 件の賞賛
返信