power dissipation for the T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

power dissipation for the T2080

946 Views
hv
Contributor II

how do we measure power dissipation for the T2080 running just one core?  thanks!

0 Kudos
5 Replies

676 Views
ufedor
NXP Employee
NXP Employee

No.

The table is for the core, not for the thread.

0 Kudos

676 Views
ufedor
NXP Employee
NXP Employee

Please refer to the T2080 Data Sheet Rev.1, Table 10. T2080 Rev 1.1 single core/single cluster low-power mode power savings, 1.0 V 105°C. The table contains power saving numbers of the dual-thread core for all lower-power states.

Please consider that disabling a core through the DCFG_CCSR_COREDISR corresponds to the PH15 power management state – i.e. resulting saving is equal to PH10 + PH15.

0 Kudos

676 Views
benjaminlux
Contributor I

If we want to estimate the power saving when disabling multiple cores. Shall we multiply the values in table 10 by the number of disabled cores ?
For example,  is the power saving resulting to the use of 1 out of 4 cores only equal to 3x(PH10+PH15) i.e 3,69 W at 1,8GHz ?

Regards,

Benjamin

0 Kudos

676 Views
ufedor
NXP Employee
NXP Employee

Yes.

0 Kudos

676 Views
benjaminlux
Contributor I

Thank you.

As there are 2 threads per core, wouldn't it even be : 3x(2xPH10+PH15) ?

0 Kudos