floating-point with mpc834x in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

floating-point with mpc834x in Linux

433 Views
rans
Senior Contributor I

Hello,

It seems that I can't use floating point in a linux application.

I checked the default configuration in the jernel build (from buildroot), and I see that PPC_FPU is selected.

Do I need to add sw emulation to kernel build ? What is missing for floating point support ?

Thank you,

Ran

0 Kudos
1 Reply

359 Views
Pavel
NXP Employee
NXP Employee

Check compilation option and compilation library for your application.

Freescale offers CodeWarrior compiler for the MPC83xx (http://www.freescale.com/tools/embedded-software-and-tools/software-development-tools/codewarrior-de...).

This compiler supports hardware and software floating point.

There is Linux GNU compiler for the MPC834x.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos