checkstop out pin in T1040

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

checkstop out pin in T1040

659件の閲覧回数
hv
Contributor II


the T1040RM listed a CKSTP_OUT_B pin but the e5500 said "The e5500 does not take a checkstop, as is the case with previous e500 cores."  what are the conditions that will cause the checkstop out pin to be asserted? 

0 件の賞賛
5 返答(返信)

514件の閲覧回数
ufedor
NXP Employee
NXP Employee

Checkstop functionality is used for debug purposes only.

The EVT signals can be used to generate checkstop in the T104x device.

0 件の賞賛

514件の閲覧回数
hv
Contributor II

I understand that checkstop is no longer associated with machine check exception in the e5500. But I would like to know what will cause the checkstop out pin CKSTP_OUT_B to be asserted?

0 件の賞賛

514件の閲覧回数
ufedor
NXP Employee
NXP Employee

Excuse me:

> The EVT signals can be used to generate checkstop in the T104x device.

You wrote:

> what will cause the checkstop out pin CKSTP_OUT_B to be asserted?

Please explain why you pose this question?

0 件の賞賛

514件の閲覧回数
hv
Contributor II

In the traditional PowerPCs, machine check was tied to checkstop. Now it no longer does. I found this reference for the P4080:

“The DACRDn, as well as DACREn and DACRRn registers along with CKSTPCR will determine what events can cause the CKSTP_OUT_N pin to be asserted.”

I would like to know the same thing for the T104x.

We are using checkstop in our software and would need to know what changes we need to make to accommodate for checktop not being there anymore. Or if there are ways we can still generate checkstop.

Thanks!

0 件の賞賛

514件の閲覧回数
ufedor
NXP Employee
NXP Employee

Excuse me, but it has alredy been written:

> Checkstop functionality is used for debug purposes only.

This means that checkstop functionality can't be used during normal processor operation.

Sorry, but additional information is available only for debug tools vendors.

0 件の賞賛