checkstop out pin in T1040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

checkstop out pin in T1040

672 Views
hv
Contributor II


the T1040RM listed a CKSTP_OUT_B pin but the e5500 said "The e5500 does not take a checkstop, as is the case with previous e500 cores."  what are the conditions that will cause the checkstop out pin to be asserted? 

0 Kudos
5 Replies

527 Views
ufedor
NXP Employee
NXP Employee

Checkstop functionality is used for debug purposes only.

The EVT signals can be used to generate checkstop in the T104x device.

0 Kudos

527 Views
hv
Contributor II

I understand that checkstop is no longer associated with machine check exception in the e5500. But I would like to know what will cause the checkstop out pin CKSTP_OUT_B to be asserted?

0 Kudos

527 Views
ufedor
NXP Employee
NXP Employee

Excuse me:

> The EVT signals can be used to generate checkstop in the T104x device.

You wrote:

> what will cause the checkstop out pin CKSTP_OUT_B to be asserted?

Please explain why you pose this question?

0 Kudos

527 Views
hv
Contributor II

In the traditional PowerPCs, machine check was tied to checkstop. Now it no longer does. I found this reference for the P4080:

“The DACRDn, as well as DACREn and DACRRn registers along with CKSTPCR will determine what events can cause the CKSTP_OUT_N pin to be asserted.”

I would like to know the same thing for the T104x.

We are using checkstop in our software and would need to know what changes we need to make to accommodate for checktop not being there anymore. Or if there are ways we can still generate checkstop.

Thanks!

0 Kudos

527 Views
ufedor
NXP Employee
NXP Employee

Excuse me, but it has alredy been written:

> Checkstop functionality is used for debug purposes only.

This means that checkstop functionality can't be used during normal processor operation.

Sorry, but additional information is available only for debug tools vendors.

0 Kudos