Toolchain with GCC 5.x series for QorIQ powerpc 32bit arch.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Toolchain with GCC 5.x series for QorIQ powerpc 32bit arch.

Jump to solution
1,271 Views
surendradhobale
Contributor III

Hello,

   We are using T1042 QorIq PPC arch processors. Currently we are using GCC4.9.3 compiler toolchain.

We are looking to upgrade the compiler for 5.x series. Is this available in any SDK?

Or How we can get that ?

Thanks,

Surendra

0 Kudos
1 Solution
803 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Surendra,

In the latest released QorIQ SDK, GCC4.9.x is still used as the default for PowerPC Architecture.

However in Linux SDK 2.0, GCC 5.2 recipes are provided, you could install SDK 2.0 and use yocto to build the binary Toolchain if necessary.

Please modify the variable GCCVERSION_qoriq-ppc as "5.2" in meta-freescale/conf/distro/fsl-qoriq.conf.

Then create a build project for T1042, and use the command "bitbake fsl-toolchain" to build the binary Toolchain.

The Toolchain is deployed in build_<board>/tmp/sysroots/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc-fsl-linux/powerpc-fsl-linux-gcc, if the building is performed successfully.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
804 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Surendra,

In the latest released QorIQ SDK, GCC4.9.x is still used as the default for PowerPC Architecture.

However in Linux SDK 2.0, GCC 5.2 recipes are provided, you could install SDK 2.0 and use yocto to build the binary Toolchain if necessary.

Please modify the variable GCCVERSION_qoriq-ppc as "5.2" in meta-freescale/conf/distro/fsl-qoriq.conf.

Then create a build project for T1042, and use the command "bitbake fsl-toolchain" to build the binary Toolchain.

The Toolchain is deployed in build_<board>/tmp/sysroots/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc-fsl-linux/powerpc-fsl-linux-gcc, if the building is performed successfully.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
803 Views
surendradhobale
Contributor III

Thanks Yiping !!!

0 Kudos