How to find the list of peripherals available on P2020RDB-PCA?
I am planning test all the peripherals or drivers from User space.
Any examples will be helpful
We are using SDK 1.7 reference manual.
Thanks.
The P2020RDB-PCA peripherals are described in the P2020RDB-PCA Specification document (P2020RDB-PCA_User_s_Guide) which has to be bundled with the board.
Please note that the most recent SDK version which supported P2020RDB-PC is 1.9, so for the devices' drivers you could refer to the:
I am going through the document that you have suggested.
From it, I can pinpoint the following peripherals:
1)Memory interface -> DDR3
2) SerDes interface -> PCIe.
3) Enhanced Local Bus Controller (eLBC) --> NOR, NAND.
3) Ethernet
4) eSPI.
5) eSDHC -> SD Card
6) GPIO
7) I2C.
8) USB
9) UART or RS232.
We are using SDK1.7, can you please provide test programs for these peripherals. We are not planning to test PCIe.
Thanks,
There are no separate tests.
U-Boot could be used for testing as a single tool.