T1042 PCIe Configuration Issue As An Endpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 PCIe Configuration Issue As An Endpoint

Jump to solution
7,096 Views
athershehzad
Contributor III

I am facing an issue related to PCIe configuration on T1042 Power PC, which is configured as an endpoint
Initially my design was working fine with one lane PCIe with 32 bit 2 GB DDR3L, now design has some changes I am looking to configure 4 lane PCIe with 64 bit 4 GB DDR3L.
Output of lspci -vv command on root-complex device gives an unassigned memory in second case. It states BAR addresses to be unassigned.
Comparing from the previous setup output of same command, BAR0 is assigned correctly, while for BAR1 it gives unassigned memory and
for BAR2 it is swapped with the memory assigned to BAR1 in previous case
Below I have attached outputs of both designs
Does anyone know how to solve this issueOutput of New ConfigurationOutput of New ConfigurationOutput of Old ConfiguaraionOutput of Old Configuaraion

 

@yipingwang  Can you please help. You have solved most my problems earlier too.

0 Kudos
1 Solution
6,949 Views
ufedor
NXP Employee
NXP Employee

Still not reverted:

fe240dd0: a0f5501f 00000000 00000000 00000000 ..P.............

Should be 17

View solution in original post

0 Kudos
16 Replies
6,845 Views
athershehzad
Contributor III

thanks @ufedor for your kind help. We could not find where this register value was being set, so we hard-coded it.

Now it is working perfectly. Thank you for time and help.

Regards Ather

0 Kudos
7,085 Views
ufedor
NXP Employee
NXP Employee

Please consider that EP BARs are configured by the EP firmware.

Please provide complete U-Boot and Linux booting logs (as text files attachments) for both configurations.

0 Kudos
7,079 Views
athershehzad
Contributor III

Thanks @ufedor for your prompt reply. Attached are the files that you have requested.

T1042rdb_v1_bootprints.txt represents Old configuration

T1042rdb_v2_bootprints.txt represents new configuration

Regards

Ather

0 Kudos
7,073 Views
ufedor
NXP Employee
NXP Employee

> I am looking to configure 4 lane PCIe

The same SerDes protocols are used in both configurations and it has PCIe1 x4 trained to x1 Gen1 - i.e. no difference.

Please provide additional information:

1) Output of lspci -vv command on RC device as text files

2) DTS files which are used in both configurations

 

0 Kudos
7,069 Views
athershehzad
Contributor III
Spoiler
SERDES protocol was set as for 4x Lane PCIe but in both cases we have disconnected 3 Lanes by removing the series capacitors in the lanes. We could not establish 4 lane PCIe connection in the previous version because of design issue but now we can have 4x lane Link, however just for testing purpose, we removed the series capacitors to check for single lane link is working or not.

Here are the files that you have requested.

Dts files were same in both cases


0 Kudos
7,049 Views
ufedor
NXP Employee
NXP Employee

Is the same DTS used?

Why different parameters for the lspci are provided for the v1:

lspci -vvvv -nn -s 03:00.0

and v2:

lspci -vvvv -nn -s 01:00.0

?

0 Kudos
7,036 Views
athershehzad
Contributor III

Yes same dts is used in both cases.

bus number is changed because in  previous version we were using a PCIe bridge that connects one root complex to two PCIe endpoint out which one endpoint is our T1042. However, in newer version we removed that PCIe bridge and directly connected root complex with endpoint(T1042).

0 Kudos
7,049 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> I am looking to configure 4 lane PCIe

Why PCIe1 is trained only to x1 Gen1?

0 Kudos
7,040 Views
athershehzad
Contributor III

It is because we have removed capacitors from series path of lane 2, 3 and 4. Hence the only established connection is of single lane PCIe, which must not be a problem since PCIe can downstream itself depending upon the connections.

Also this is done only for debugging purpose.

 

0 Kudos
7,029 Views
ufedor
NXP Employee
NXP Employee

Please capture in U-Boot PCIe1 registers (CCSR range 0x24000-0x24F00) dumps for both configurations.

0 Kudos
7,015 Views
athershehzad
Contributor III

Attached txt files are U-Boot PCIe1 registers (CCSR range 0x24000-0x24F00) dumps for both configurations

v2 is for new design 

v1 is for old design

0 Kudos
7,011 Views
ufedor
NXP Employee
NXP Employee

V1

fe240dc0: 0007e000 00000000 00000000 00000000    ................

fe240dd0: a0f55017 00000000 00000000 00000000    ..P.............

V2

fe240dc0: 000fdff0 00000000 00000000 00000000    ................

fe240dd0: a0f5501f 00000000 00000000 00000000    ..P.............

Why is this difference?

0 Kudos
7,005 Views
athershehzad
Contributor III

This was changed in drivers file for DDR changes (from 2Gb to 4Gb). I thought this change would fix the memory unassigned issue as we assumed that for 4gb ddr we have to set registers accordingly, but it didn't. Forgot to revert the changes. What do you propose I should have done?

0 Kudos
6,994 Views
ufedor
NXP Employee
NXP Employee

Revert the changes.

0 Kudos
6,983 Views
athershehzad
Contributor III

Output with changes  revert, still same behaviour 

0 Kudos
6,950 Views
ufedor
NXP Employee
NXP Employee

Still not reverted:

fe240dd0: a0f5501f 00000000 00000000 00000000 ..P.............

Should be 17

0 Kudos