T1040 L2 Switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,034件の閲覧回数
vsv
Contributor III

We have a requirement to build a switch solution for which we are considering to leverage on the L2 switch core available in T1040 processor.

The customer has asked for support of around 12-14 ports in a switch. Since the initial PoC is going to be developed with T1040RDB that has 8 ports available outside, we are planning to recommend the customer to have two RDB boards cascaded one over the other.

If we connect the 8 ports available in the RDB with end systems (server class machines, desktop PC's etc.), can we use one out of the remaining 3 ports that is available in addition, to cascade to the second switch - in which we can connect the remaining end systems.

Will this sort of topology work in making an end system connected to Switch 1 communicate with an end system connected to Switch 2?

We intend to have the end systems connected within the switch to have their communication done by the L2 switch core whereas the end systems connected to these two different switches get communicated over the T1040 processor outside the L2 Switch core?

Thanks in advance

タグ(2)
1 解決策
781件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, this configuration is possible.

元の投稿で解決策を見る

1 返信
782件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Yes, this configuration is possible.