[SPI] SPI 1/ 3 port setting of lx2160a in the RCW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[SPI] SPI 1/ 3 port setting of lx2160a in the RCW

684件の閲覧回数
DohwanAhn
Contributor II

 

Our board is based on LX2160a and we are configuring SPI1/SPI3 as Master and using it for communicating with the Slave.

For this purpose in the RCW we have configured SDHC1_BASE_PMUX=2 ( 0b'010 - SPI1_SOUT, SPI1_PCS[0:2], SPI1_SCK, SPI1_PCS[3]) for SPI1. But, we can't find SPI1_SIN in the RCW.

In the case of SPI3, we have configured SDHC1_DS_PMUX=2 (0b'10 - SPI3_SCK) , IIC5_PMUX=3 (0b'011 - {IIC5_SCL, IIC5_SDA} ={ SPI3_SOUT, SPI3_SIN}). But, we can't find SPI3_PCS0 in the RCW.

How can we set up RCW to use SPI1 and SPI3 fully?

 

タグ(3)
0 件の賞賛
返信
0 返答(返信)