LTIB or BITBAKE...which is better?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB or BITBAKE...which is better?

598 Views
sharathchandra
Contributor II

I have P4080 board, which is better/recommended to use to build the images...is it SDK from Yocto Project containing containing Bitbake (or) an .iso which contains LTIB?

0 Kudos
2 Replies

443 Views
alexander_yakov
NXP Employee
NXP Employee

I've answered this question already in Service Request. Shortly - if you have P4080 board from third-party vendor, than this board in not guarantied to be supported by our Linux SDK, and you have to use Linux BSP supplied with board by board vendor.

We use bitbake in our Linux SDK, but your board vendor may use LTIB in its Linux BSP for this board.

443 Views
lunminliang
NXP Employee
NXP Employee

If your P4080 is rev 3, you need to use Yocto SDK 1.3 or later version as this is not supported in previous SDK.