attached err snapshot:
CodeWarrier: CW_CW4NET_v2018.01_Win_b180126_Offline
steps
1.Hw setting configured exactly as CodeWarrier’reademe
2.modfy USE_SAFE_RCW = True in Taget Initiaialization File
Readme file setting
#-------------------------------------------------------------------------------------#
# Switch settings for LS2088A QDS - PCB REV B2, FPGA REV V12
#-------------------------------------------------------------------------------------#
NOR_BOOT:
---------
SW1 : 0x12 = 00010010 SW5 : 0xFF = 11111111 SW9 : 0xFE = 11111110
SW2 : 0xFF = 11111111 SW6 : 0x0F = 00001111 SW10: 0xE8 = 11101000
SW3 : 0x2E = 00101110 SW7 : 0x2A = 00101010 SW11: 0xFC = 11111100
SW4 : 0xAF = 10101111 SW8 : 0x49 = 01001001 SW12: 0xFF = 11111111
Where '1' = UP/ON
#-------------------------------------------------------------------------------------#
# JTAG configuration and setup
#-------------------------------------------------------------------------------------#
CFG_JTAG_ROUTE needs to be configured as below:
SW10[6:8] = 000 - CCS to DUT Only
Including the QIXIS FPGA on the JTAG chain is not currently supported.
Also TBSCAN_EN_B needs to be configured as below:
SW5[7] = 1 - Debugger mode
Ccs diagnostic information
(bin) 51 % source IDcode.tcl
Scanning for available TAPs connected via USB.....
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+
+ Available Remote Connections
+
+ 1 - CodeWarriorTAP - 00:04:9f:04:2b:70
+ 2 - CodeWarriorTAP - <Specify IP Address>
+ 3 - GigabitTAP - <Specify IP Address>
+
+ x - Exit Script without Changes
+
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Specify connection:
2
Specify IP Address
10.192.208.173
Configuring TAP Interface....
Configured Connection: cwtap : 10.192.208.173
TDO -----
|
* Device 0 IDCODE: 5133001D Device: NXP QIXIS
|
TDI -----
###################################################
#
# configTAP - Redefine TAP interface
#
# scanboard - Scans the target system
# and returns the JTAG IDCode
#
# ir - Loopback test
#
###################################################
(bin) 52 %
Can someone help me see this question?