Boot strapping an LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot strapping an LS1043A

635 Views
yaronalterman
Contributor II

Hello, I am trying to write some basic bootstrap code for an LS1043A processor.

At reset the processor comes up at EL3/secured of course, and I would like to bring it to a none-secure EL1 and branch to my application from there.

At first I need (to my understanding) to transition to EL2/non-secure on the way to EL1.

Configuring the SCR_EL3 register goes well, and so I get to EL3/non-secure mode. 

I then configure the SPSR_EL3 with 0x3c9 (9 being the encoding for EL2 using it's stack pointer), and ELR_EL3 with my EL2_entry address. Then I call eret.

What happens next is I get a sync external instruction abort.

Any idea why this is happening? any help would be appreciated.

Thank,

Yaron

Code snippet:

mov x0, #0x501 //aarch64 + non - secure state

msr scr_el3, x0 //move to non-secure state

mov x0, #0x3c9 //prepare transition to EL2

msr spsr_el3, x0

adr x0, el2_entry

msr elr_el3, x0

eret

1 Reply

497 Views
yaronalterman
Contributor II

OK, got it.

Need to configure the flash memory as non-secure via the CSU before going into EL2 non-secure mode, otherwise the memory is not accessible.

Since I am going baremetal here (no u-boot to configure stuff for me), I have to do all the configurations myself, and this one escaped me.