i have bug during booting process it shows jffs2 dies with inflate returned -3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i have bug during booting process it shows jffs2 dies with inflate returned -3

1,146 Views
madhukumar
Contributor I

hi ,

operating system : fedora 12

tool : LTIB - 2008

kernel version : linux-2.6.25

i bug with during booting process it stop at VFS: Mounted root (jffs2 filesytem)

please find the attached Booting.docx and please suggestion.

Labels (1)
Tags (1)
0 Kudos
3 Replies

665 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

The Processor Expert Software forum is related to this tool issues.

Could you specify the issue you have more precisely? What do you use (MCU/MPU, drivers and so on) and what can cause the problem you have reported, please?

I will move your question to correct place. See for example discussion about Fedora OS in the thread Install Fedora linux to QorIQ

Best Regards,

Marek Neuzil

0 Kudos

665 Views
madhukumar
Contributor I

hello Marek,

we used MPU drivers for MCF5485 processor are configuration LTIB-2008 tool, after power on during rootjffs2 image file copied from flash to ddram at the error cooured

error message as shown below following lines

VFS: Mounted root (jffs2 filesystem)

inflate returned -3

unable access at virtual address e304186 aps: 00000000

PC: [<001090b8>] zlib_inflate+0x738/0x14f0<0>

please give suggestion

0 Kudos

665 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I am sorry I am not able to resolve this issue (i). I also see that this issue is replicated and answered  in the ColdFire/68K Microcontrollers and Processors space

(see booting issueVFS: Mounted root (jffs2 filesystem) inflate returned -3 unable access at virtual addre... issue).

I will close this issue.

Best Regards,

Marek Neuzil

0 Kudos