hi ,
operating system : fedora 12
tool : LTIB - 2008
kernel version : linux-2.6.25
i bug with during booting process it stop at VFS: Mounted root (jffs2 filesytem)
please find the attached Booting.docx and please suggestion.
Hello,
The Processor Expert Software forum is related to this tool issues.
Could you specify the issue you have more precisely? What do you use (MCU/MPU, drivers and so on) and what can cause the problem you have reported, please?
I will move your question to correct place. See for example discussion about Fedora OS in the thread Install Fedora linux to QorIQ
Best Regards,
Marek Neuzil
hello Marek,
we used MPU drivers for MCF5485 processor are configuration LTIB-2008 tool, after power on during rootjffs2 image file copied from flash to ddram at the error cooured
error message as shown below following lines
VFS: Mounted root (jffs2 filesystem)
inflate returned -3
unable access at virtual address e304186 aps: 00000000
PC: [<001090b8>] zlib_inflate+0x738/0x14f0<0>
please give suggestion
Hello,
I am sorry I am not able to resolve this issue (i). I also see that this issue is replicated and answered in the ColdFire/68K Microcontrollers and Processors space
(see booting issueVFS: Mounted root (jffs2 filesystem) inflate returned -3 unable access at virtual addre... issue).
I will close this issue.
Best Regards,
Marek Neuzil