PT2000 Dev brd stops working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PT2000 Dev brd stops working

1,505 次查看
frevoredo
Contributor I

I'm using the PT2000 programmable Solenoid Controller Gate Driver eval board with a 24V battery supply. I've upgraded the devices n the board to handle 24V system.  It works for a couple of minutes and then suddenly stops communicating. I have an external VCCP and the VCCP_EXT_EN register set to 1 as explained in the datasheet. After a couple of configuration attempts the chip stops responding to SPI commands and does not recover.

Anyone have any ideas as to what may be wrong??

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,331 次查看
frevoredo
Contributor I

Further investigations shows the STARTx input is shorted to ground. I suspect this is caused when power is removed from the board with the START signal still present or when the START signal is present before power to the PT2000. At the moment the START signal is generated by another unit and is feed into the PT2000. I have to make sure the PT2000 is powered up first and down last.

0 项奖励
回复

1,331 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Frank,

You should get a direct answer from my colleague Pierre. If not, please let me know and I will follow up.

Regards,

Tomas

0 项奖励
回复

1,331 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Frank,

I am asking our device group to comment on this and will update this thread when I get their feedback.

Best regards,

Tomas

0 项奖励
回复