[mpc8569e] Rapidio signal quality low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[mpc8569e] Rapidio signal quality low

Jump to solution
885 Views
jiag
Contributor I

1 daughter board (where mpc8569e located) is connected to a motherboard via a connector and motherboard connects backplane via anther connector. On system power up, Rapidio reg 158 sometimes shows 01, which means port is un-initialzed. Per eye-diagram shows, the Vdiffpp of Rapidio signal through the connector which connects motherboard to the backplane is about 800mv, seems it will get even worse when adding the backplane attenuation, and the Rapidio signal entering the tsi578 switch may be weaker than the lower bound specified in the spec.

Since there'r two Rapidio transmitter type (long run and short run), we guess to configure the transmitter to long run may improve the signal quality, but unfortunately we haven't find the right register, we use MPC8569 btw.

My question: Is there a regiter that configure the Rapidio transmitter type? Or are there some hardware design related issue that may cause our problem?

0 Kudos
1 Solution
772 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

No, there isn't a register that configure the Rapidio transmitter type, if you try a link that is classified as "long-run"
(as described by the SRIO spec based on length of the traces), you should follow the board/trace layout parameters described in
the EC for a "long-run" link and design your board accordingly.

View solution in original post

0 Kudos
1 Reply
773 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

No, there isn't a register that configure the Rapidio transmitter type, if you try a link that is classified as "long-run"
(as described by the SRIO spec based on length of the traces), you should follow the board/trace layout parameters described in
the EC for a "long-run" link and design your board accordingly.

0 Kudos