Linux Driver for QE UMCC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Driver for QE UMCC

2,364件の閲覧回数
aleksandargeras
Contributor I

Hello,

 

We are currently working on a product based on T1040, and we are planning to use QE UMCC for implementing TDM link.

We are estimating needed effort for implementing this in Linux Kernel, so far we have seen that there is no available UMCC driver.

 

So our question is:

Is there currently publicly available Linux Kernel driver that uses UMCC functionality, or is there a plan in near future such a driver to be available?

 

Regards,

Aleksandar

0 件の賞賛
返信
3 返答(返信)

2,088件の閲覧回数
tedfriedl
Contributor I

Aleksandar,

How did you do with this project?  I'm doing the same now for VxWorks. I think I have most of the UMCC/SI/TDM figured out for my application except for the commands to the UMCC through the CECR register.  NXP's discussion about this in the Rev 8 QEIWRM is sparse and seems contradictory.

 

Ted Friedl

0 件の賞賛
返信

2,088件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use SDK 2.0 for the T1040 board. Look at kernel menu configuration from this SDK.

 

Device Drivers  --->            

[*] Wan interfaces support  --->    

<*>   Generic HDLC layer       

<*>     Freescale QUICC Engine HDLC support


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,088件の閲覧回数
aleksandargeras
Contributor I

Hi Pavel,

Thanks for your answer, we are aware of fsl_ucc_hdlc driver, the question is not regarding ucc hdlc driver.

We are planning to use umcc (replacement for mcc in T1040 QuiccEngine) for implementing 8 independent 2Mbps

TDM lines using UMCC and one of the available TDMs (TDMA or TDMB).

Current kernel QE support (drivers/soc/fsl/qe) already provides interface (examples) for configuring some of the QE subsystems (UCC slow, tdm, muram, also there is ucc_uart driver avilable) but there is no interface (example) for using UMCC.

So this specific question is related exactly to UMCC usage and current Kernel support availability.

It would be of help if any kind of PoC kernel driver, or configuration example in any other form is available beside

what is described in QE documentation.

Regards,

Aleksandar

0 件の賞賛
返信